cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I beg your pardon, there are many details so I wrote in a Word document. I would like to thank you for your kind assistance. Eli shaul

Eshau
Associate
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mon2
Senior III

Hi. Short answer - as far as I know this target kit is not yet properly supported with the toolchain. The stable kits are the ones with V2.0 templates. The version 1.x are often just broken.

Please do review this thread which may help - especially the posting by Martin (who is one of the s/w developers of the TouchGFX tool):

https://community.st.com/s/question/0D70X0000076nTR/stm32l4r9ieval-with-dpi-480x272-lcd-application-template?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vr0X&emtm=1551739791440&fromEmail=1&s1ext=0

Hope this helps.

Eshau
Associate

Hello,

Thanks for your response.

The TouchGFX generated the code just fin And as I mentioned I can build and run the project from Microsoft VS2017 Without any problems.

All I ask is to try to convert the project to CMmake package. https://cmake.org/

The purpose is to combining CMake files to work with VisualGDB.

I forgot to send the file CMakeLists.txt

Thanks

eli shaul