cancel
Showing results for 
Search instead for 
Did you mean: 

hello guys. i work with touch GFX but i have a question. can i startup a 7" LCD with stm32f469i eval? if yes how?

HBalo.1
Associate

and more, how the characteristic parameter this LCD has?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Alexandre RENOUX
Principal

Hello,

What is this 7'' LCD ? Because it's not the one embedded on the F469-EVAL.

Please provide more information.

/Alexandre

HBalo.1
Associate

In fact, I designed my work in touchgfx software on stm32f469 eval.

Now if I design a board exactly like the stm32f469 eval board and put a 7-inch lcd with a resolution of 480 x 800 on it, according to the touchgfx settings, will the code generated by touchgfx run on this hardware?

And my question is exactly what 7-inch LCD should I get so that I do not get into trouble?

Will the problem be solved just by changing the settings of the LTDC unit according to the 7-inch LCD?

Alexandre RENOUX
Principal

Hello,

Yes in theory the code generated by CubeMX and TouchGFX should work.

For the screen, we don't have any recommendation in particular. If you choose a LTDC screen, this will simplify the implementation as LTDC is fully handled by TouchGFX Generator.

/Alexandre

mehmet06
Associate II

I want to use a 7 inch and above screen with toucgfx and you do not know which screen I can use. So what use will this kit be if I can't make an original design and I can't even find the screen on it? I paid a ton of money for the stm32f469 i kit.