Skip to main content
frackers
Senior
December 3, 2019
Question

Hardware JPEG mixing encode and decode

  • December 3, 2019
  • 1 reply
  • 571 views

So who was the bright spark who decided that both encode and decode should use the same callback function names? Duh! Means I can't even make them static to isolate them! Doesn't the JPEG hardware know whether its doing an encode or a decode?

Also, the JPEG utilities have compile time (rather than run time) selection of the image format. So much for encoding RGB565 from a camera and decoding ARGB8888 for animations.

Not happy having to play with (yet more) DMA2D format conversions to address the inadequacy of the interface

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
December 3, 2019

I don't think the architects/coders here are particularly sophisticated. Let alone familiar with complex requirements of streaming audio/video pipelines, or the system level scope.

Can't you readily overload the context structure/handle passed to the callbacks? You can hide a lot of your per-instance information in there. If you really don't like the library code, refactor it.

If I were you I'd find some of the engineers responsible for the software and IP integration to discuss this with. You're kind of outside the envelope for front line support engineers/developers.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..