Font Dither Adjustment
I am having a problem with on-screen fonts. The dither/font-smoothing applied to the fonts eats into thin segments of the characters too much. This causes them to be too dim on screen for my application.
I've managed to show that the problem clears up if I use the BOLD version of the same font when defining my typographies, so it seems related to how the dither algorithm behaves around thin sections of characters.
When BOLD, the dither doesn't touch the core of the character at all, its a bright, solid colour. When not bolded, there are lots of little tracks of dim pixels winding through the main body of the character.
I would prefer not to resort to using the BOLD typeface everywhere if possible.
Are there any settings I can adjust to "sharpen" the text or limit how much dither bleeds into the body of the character? I'm running 4.15.0.