2013-10-13 10:50 AM
Hi 🙂
As usual 'Murphy law' i get little problem .... I have connect 3 different USB Stick on 3 Different F429 Disco Board though the microSD connector with no results. I then tried with a USB connector directly connected to the USB dedicated pins with the same no results :( Is it something special to do to made it work ?? From the docs i doesn't see anything special to do for the micro usb port , i have think it will be functional directly with the provided demo ... I formatted them in fat16 and fat32 for be sure and they are 1,2 and 4Gb. Cheers. #discovery #stm32f429 #lcd-tft2013-10-16 11:52 AM
I tried to put 8Mhz on the HSE, same result.
OK, I will open a new topic about USB device VCP.Thanks for your help.2013-10-16 12:41 PM
Do you mean ''it is working'' ?
2013-10-16 12:56 PM
Do you mean ''it is working'' ?
It appears to be functioning. Edit#1 Seems to crash when disconnected, will need to dig into that. Edit#2 See how to resolve that