Enabling Ethernet on the STM32H745I-DISCO Board with TouchGFX Integration
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-03 8:46 AM
Hello,
I’m working on a project with the STM32H745I-DISCO board and need to utilize the Ethernet interface on the M4 core.
I’ve created a graphical application using TouchGFX that runs on the M7 core, and a user application that runs on the M4 core, using STM32CubeIDE. The generated code indicates a dependency on QUADSPI libraries for the TouchGFX framework. However, according to the User Manual UM2488, to enable Ethernet, SB3 and SB4 must be connected, and resistors R38 and R40 need to be removed. This configuration would disconnect the QUADSPI, creating a conflict with the requirements for TouchGFX.
Given these constraints, what is the best way to configure Ethernet on the STM32H745I-DISCO board without disrupting the necessary connections for TouchGFX?
Kind regards,
Frosty
- Labels:
-
STM32CubeMX
-
TouchGFX
-
TouchGFX Designer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-03 8:57 AM
Hello @frosty ,
this conflict between QUADSPI and Ethernet is only present in MII mode thus this constraint :
For 10 Mbit/s half-duplex MII communication, SB3 and SB4 must be ON.
you can try to configure Ethernet in RMII mode that will not use these pins:
RMII pinconfig is as follows for STM32H745I-DISCO:
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-02-25 12:08 PM
@frosty I am looking for an example project that does exactly what you described. Do you happen to have a github repo for this configuration? I am very new to the CubeIDE so any help would be appreciated. Thanks!
Adam