cancel
Showing results for 
Search instead for 
Did you mean: 

Dynamically add containers to swipe container at runtime

NPr
Associate II

Hello,

ic want to add container dynamically at runtime. For example I want to create new containers an delete old once. My first try was to allocate an object on the heap an store the pointer in the class object. But if a add them to a container the chip hangs up.

Is there anyone with experience in this field?

Thank you for help.

BW NPr

3 REPLIES 3
FTkal.1
Associate II

That should all be possible. The library doesn't care if your objects are on the stack or on the heap.

Stopping in the debugger after the hang will often show you have stopped at an assert() statement.

NPr
Associate II

My problem was an allocation error. Because I use FreeRTOS and C++. And the new operator wasn't overloaded.

Thank you for your help!

ferro
Senior III