cancel
Showing results for 
Search instead for 
Did you mean: 

install programm in linux docker container quietly (no interaction)

econner-cog
Associate

I'm trying to install 

./SetupSTM32CubeProgrammer-2.21.0.linux -q 

But it just keeps failing or waiting for user response.  Its not quiet if it asks for interaction.  Moreover I have a tried a varfile but it expects a specific format (XML? Schema?)

I can't find any documentation on how to install this without user interaction.  Can anyone help or point me to the documentation?

 

Thank you 

1 ACCEPTED SOLUTION

Accepted Solutions
Kouthair
ST Employee

Hello there!

To install STM32CubeProgrammer without user interaction, you could refer to the UM2237: 1.2.8 Automatic/Silent installation mode.

I'll also attach an XML auto-install file with the structure needed for the automatic installation, you can generate this script during the final installation phase using the interface to capture the configuration and preferences selected during the installation process.

Please let us know if you need further assistance.

Kouthair.

If a post has helped you, make sure to mark it as a solution.

View solution in original post

1 REPLY 1
Kouthair
ST Employee

Hello there!

To install STM32CubeProgrammer without user interaction, you could refer to the UM2237: 1.2.8 Automatic/Silent installation mode.

I'll also attach an XML auto-install file with the structure needed for the automatic installation, you can generate this script during the final installation phase using the interface to capture the configuration and preferences selected during the installation process.

Please let us know if you need further assistance.

Kouthair.

If a post has helped you, make sure to mark it as a solution.