DCMI only triggering line interrupt
I have an OV7670 camera that I am trying to capture images with. I am able to communicate with and set registers for the camera. When power, GND, and XLCK (16 MHz) pins are supplied to the pin I am also able to detect that proper image data is being sent via a logic analyzer.
When acquiring the image (via HAL drivers), I only ever receive an infinite amount of "Line Interrupts" which execute the callback function HAL_DCMI_LineEventCallback. Whether I try to perform an acquisition in snapshot or continuous mode, I still receive an infinite amount of these interrupts. I also never receive any other interrupts or error functions. What could be causing this?
Shouldn't I only ever receive the amount of line interrupts associated with a single image in snapshot mode? I believe I have enabled all DCMI interrupts, is this not the case? Why am I not receiving any other interrupts? Could this be an error on the DMA side of things?
If I understand this code correctly, once the snapshot has been taken the pixel data should simply be allocated in the data_buffer variable?
DCMI Initialization:
void HAL_DCMI_MspInit(DCMI_HandleTypeDef* hdcmi)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hdcmi->Instance==DCMI)
{
/* USER CODE BEGIN DCMI_MspInit 0 */
/* USER CODE END DCMI_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_DCMI_CLK_ENABLE();
__HAL_RCC_GPIOE_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/**DCMI GPIO Configuration
PE4 ------> DCMI_D4
PE5 ------> DCMI_D6
PE6 ------> DCMI_D7
PA4 ------> DCMI_HSYNC
PA6 ------> DCMI_PIXCLK
PC6 ------> DCMI_D0
PC7 ------> DCMI_D1
PC8 ------> DCMI_D2
PC9 ------> DCMI_D3
PB6 ------> DCMI_D5
PB7 ------> DCMI_VSYNC
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF13_DCMI;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* DCMI DMA Init */
/* DCMI Init */
hdma_dcmi.Instance = DMA2_Stream1;
hdma_dcmi.Init.Channel = DMA_CHANNEL_1;
hdma_dcmi.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_dcmi.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_dcmi.Init.MemInc = DMA_MINC_ENABLE;
hdma_dcmi.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
hdma_dcmi.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
hdma_dcmi.Init.Mode = DMA_NORMAL;
hdma_dcmi.Init.Priority = DMA_PRIORITY_LOW;
hdma_dcmi.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_dcmi.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_dcmi.Init.MemBurst = DMA_MBURST_INC4;
hdma_dcmi.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_dcmi) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hdcmi,DMA_Handle,hdma_dcmi);
/* DCMI interrupt Init */
HAL_NVIC_SetPriority(DCMI_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DCMI_IRQn);
/* USER CODE BEGIN DCMI_MspInit 1 */
/* USER CODE END DCMI_MspInit 1 */
}
}Main Function:
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_DCMI_Init();
/* USER CODE BEGIN 2 */
Delay_Init(); //Set up sccb delay pins
BB_SCCB_HardwareInit(); //set up sccb communication pins
Init_OV7670(); //write camera registers to desired values
uint32_t data_buffer; //define buffer to store pixel data
HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, data_buffer, 320*240/2); //capture in snapshot
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}