cancel
Showing results for 
Search instead for 
Did you mean: 

Changing the DSI_TE pin in the STM32F469 (tearing effect)

Mohamed eleuche
Associate II
Posted on July 22, 2017 at 18:45

Hello everyone,

I am using the STM32F469i-disco for my touch screen project and I was able to modify the sample example in the STM32Cube_FW_F4_V1 to satisfy my project. ( ..\STM32Cube_FW_F4_V1\Projects\STM32469I-Discovery\Examples\BSP) Now I am trying to use the STM32F469BIT6 (TQFP176 ) instead of the BGA one used in the Discovery board.

My problem is I do not find a way to change the DSI_TE pin in the Library from PJ2. I looked everywhere in the code but I do not find it. 

Thank you for your help

#stm32f469i-disco #stm32f469-dsi #tearing-effect
2 REPLIES 2
Yi?it Uyan
Associate II
Posted on July 22, 2017 at 19:30

Hi

eleuche.Mohamed

, what is the tearing effect you mentioned in the question?

(I'm having a similar issue on the same board, maybe they might be related..)

Posted on July 23, 2017 at 10:17

The tearing effect is an effect similar to judder.

It is the pin 22 of the LCD module connector CN10 (TE), since the 

STM32F469BIT6 (TQFP176 ) does not have PJ2, I need to move it to another port and I need to change the pin in the software!

0690X00000607dOQAQ.png