cancel
Showing results for 
Search instead for 
Did you mean: 

Can you turn textareas upsidedown?

Sandy.Dahl
Associate II

Is it possible to turn textareas upsidedown without having to use texturemapper?

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

In the property settings of a textArea widget in Designer, you can set the rotation angle of your widget : 0° ("normal"), 90°, 180° and 270°. I believe you are looking for the 180degree rotation. If you wish other angles and you do not need to modify your text then I would recommend to not use a textArea but a texturemapper like you said.

0693W000007DxJzQAK.png 

/Romain

View solution in original post

4 REPLIES 4
Romain DIELEMAN
ST Employee

Hi,

In the property settings of a textArea widget in Designer, you can set the rotation angle of your widget : 0° ("normal"), 90°, 180° and 270°. I believe you are looking for the 180degree rotation. If you wish other angles and you do not need to modify your text then I would recommend to not use a textArea but a texturemapper like you said.

0693W000007DxJzQAK.png 

/Romain

Was it enough for your project ? I found a project of mine with a custom widget to rotate the text at any angle if you wish.

/Romain

Sandy.Dahl
Associate II

Hi @Romain DIELEMAN​ ,

thanks for your answer, that was exctly what I was look for!

Kind regads,

Sandy

Perfect :thumbs_up: