cancel
Showing results for 
Search instead for 
Did you mean: 

Can I use the STM32F429IIT6 and ST7789vi LCD Controller?

dark_knight
Associate

Hi,

I am working on a TouchGFX project, which connects my STM32F429IIT6 with a custom board with 2.4" TFT display. The Display include a ST7789vi chip and uses the 16-bit (RGB-5-6-5) input. I have found the STM code for the st7789h2.

How do I get the right format for transferring the pixels from the framebuffer memory to the display?

Thanks

0 REPLIES 0