cancel
Showing results for 
Search instead for 
Did you mean: 

Can I name the screen ADJUST and Box With Border adjust?

AD�?b
Senior

I have a problem with Tutorial 2. I don't want to add the counter after pressing. Does not work after implementation " Using a wildcard text " ?

16 REPLIES 16

Hi Martin.

For now, I'm studying "Connecting the UI to your system". When I'm done, I will read what you have proposed.

At the moment I have upgraded CubeIDE 1.1.0 to 1.2.0 and I can't load the configurator and I need to because I will need it for the I / O setting. Now I will reinstall CUBEIDE 1.2.0 and configure my program from the beginning.

By "Configurator" do you mean the CubeMX Configurator from within CubeIDE?

/Martin

New CubeIDE 1.2.0

But by "Configurator" do you mean the MCU configurator module in CubeIDE? (CubeMX plugin)

I installed CubeIDE 1.2.0. There is no touchGFX there?

Not sure what you mean. Do you mean inside the MCU configurator? Did you read the sticky on release 4.13.0 of Touchgfx and CubeMX 5.5.0 (in which TouchGFX middleware was replaced with the TouchGFX Generator CubeMX addon through X-CUBE-TOUCHGFX 4.13.0)

I work in STM32CubeIDE 1.1.0. When I updated to STM32CubeIDE 1.2.0 I didn't have a touchGFX.