2021-09-02 7:20 AM
Hi!
Since upgrading to TouchGFX 4.17, a box with an Alpha value does not work anymore. It just paints like as an opaque box, but not like a (semi-)transparent box.
Thus I tried to create my own widget that draws a rectangle with the following code:
HAL::getInstance()->lcd().fillRect(invalidatedAreaAbsolute, color, alpha);
But when alpha > 0, the rectangle is NOT (semi-)transparent, but opaque.
How can I get the alpha working with TouchGFX 4.17?
KR, Klemens
2021-09-06 2:27 AM
Hum that is strange. Alpha does work in my projects. Are you working on a custom hardware or on one of ST development kit ?
Could you share photos/screenshots or your project so that we can have a better idea of what you are facing ?
/Romain
2021-09-07 1:54 AM
Not an answer but I'm having the exact same issue on STM32H7B3 Discovery Kit on TouchGFX Designer 4.17, the simulator built from this has alpha but when running on the actual board it does not. This worked correctly on the board in 4.15 which I recently upgraded from.
Edit: only affecting box and box with border (circle and shape work correctly), for my use case I'm just dropping them on the canvas and setting the alpha there, I'm not creating them dynamically)
2021-09-07 5:16 AM
Hi,
Could you share your project ?
/Romain
2021-09-07 5:19 AM
It is a bit tricky because it is very large, I would make a simple demo but as you saw from my other ticket I can't make a new project at the moment. I will see if I have the modal window example I can update to 4.17 as I imagine it does the same. Alternatively take any of the examples and dump a semi-transparent box on the main screen.
2021-09-07 5:32 AM
2021-09-07 5:32 AM
2021-09-07 5:55 AM
When first running your project on 4.17 it didn't work as you explained. I then opened the ioc file with STM32CubeMX 6.3.0 and saw that it was not using the latest FW package v1.9.0 (and would not recognize that the one used, v1.6.0, was not the latest). So I changed that manually (by opening the ioc file with notepad++ and editing the FW package version), generated code and now it works. I will not lie, I do not understand why this old firmware package makes the alpha not work with TouchGFX 4.17... The latest version of the STM32H7B3dk TBS available in TouchGFX 4.17 uses the FW package 1.9.0 so use this one instead when we find a solution to your other issue :grinning_face_with_sweat: or make sure you use the latest FW package when starting a project with TouchGFX 4.15
/Romain
2021-09-07 5:58 AM
Thanks for that, I will try the same manual change you made is there a "proper" way to update/get the FW package (or should I just get it when installing TouchGFX Designer)?
2021-09-07 6:03 AM