cancel
Showing results for 
Search instead for 
Did you mean: 

4.11 Can not create/open project

DJin.3
Associate

I check the log, it will pop this error:

System.ArgumentException: 已添加了具有相�?�键的项。(An item with the same key has already been added)

  在 System.ThrowHelper.ThrowArgumentException(ExceptionResource resource)

  在 System.Collections.Generic.Dictionary`2.Insert(TKey key, TValue value, Boolean add)

  在 TouchGFXDomainModel.FontGetter.GetAvailableFonts()

  在 TouchGFXDomainModel.LoadSave.Excel.TextDB.ReadFromExcelFile(String path)

  在 TouchGFXDomainModel.LoadSave.Serial.FromSerial.Convert(SerialApplication a)

  在 TouchGFXDomainModel.LoadSave.Serial.FromSerial.Convert(SerialModel m)

  在 TouchGFXDomainModel.LoadSave.LoadSave.Load(String filename)

  在 TouchGFXPackages.ImportExport.ImportGui.GetModel(FileInfo fileInfo)

  在 TouchGFXPackages.PackageManager.CombineAtAndUi(TouchGFXPackage tgui, TouchGFXPackage tgat, String projectPath, String applicationName, Int32 height, Int32 width, ColorDepth selectedColorDepth, Action`2 progress)

  在 TouchGFXDesigner.StartupWindow.MyApplications.CreateNewApplicationViewModel.<>c__DisplayClass89_0.<CombinePackagesAsync>b__0()

  在 System.Threading.Tasks.Task`1.InnerInvoke()

  在 System.Threading.Tasks.Task.Execute()

1 REPLY 1
Martin KJELDSEN
Chief III

Hi @DJin.3​,

4.11 isn't out officially, so you must have gotten it from someone here at the office :) Try opening your excel file - is it corrupt? This error, i think, comes from an excel library we're using.

/Martin