2020-12-02 4:56 AM
When comparing installation results with contents of Security_WS_Tools_Installation.pdf, there are the following inconsistencies:
2020-12-02 5:13 AM
Hello Rongal,
1) when you launch the installer it will try to install STM32CubeProgrammer v2.5.0
STM32SecuWS-material.exe
> STM32CubeProgrammer 2.5.0
> STM32CubeIDE 1.4.2
> STM32SecuWS material
If this binary propose to install the v 2.4.0, you don't have download the package recently ( it has been updated in September).
Then if you already have a STM32CubeProgrammer v2.4.0 , you may just need to update the path in C:\STM32SecuWS\Tools\Other\SetEnv.bat
This is describe in the sklide 20 of the installation guide
2 . It was the installer that will create all the C:\CSTM32SecuWS\L4 sub structure . No zip file here.
the only zip file in this installation process is STM32CubeExpansion_SBSFU_V2.4.0.zip this one must be unzip at location C:\STM32SecuWS\L4
I would advise to Erase the folder C:\STM32SecuWS
and launch again the installer and check the status.
Best regards,
Frantz
2020-12-02 11:35 PM
2020-12-02 11:38 PM
You should have the link in the invitation with the material but I send it again just now.
Talk to you soon.
Frantz
2020-12-02 11:48 PM