ThreadX secure stack with Secure Manager
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 3:32 AM
Hello,
We are using an STM32H573 with the Secure Manager provided by ST running in the secure environment. In the non-secure environment, we are calling PSA functions. These calls work before ThreadX is launched but fail afterward.
According to the page Introduction_to_THREADX#STM32_integration, when TrustZone is enabled, I need to use a secure stack for each thread calling functions from the secure environment. To implement secure stacks, the functions defined in tx_thread_secure_stack.c should be added to the secure environment.The example STM32Cube_FW_H5_V1.4.0/Projects/NUCLEO-H563ZI/Applications/ThreadX/Tx_SecureLEDToggle_TrustZone illustrates this but without using the Secure Manager.
However, I need to use the Secure Manager. Can you provide some guidance ?
- Are the functions from the file tx_thread_secure_stack.c included in the Secure Manager ? If so, how can I call them ?
- Should I create a secure module with the SMDK for this ?
Thank you in advance for your support!
Best regards
Quentin
- Labels:
-
Secure Manager
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 6:56 AM
Hello @QuentinWit ,
The Secure Manager is not re-entrant. You need to ensure that only one call to Secure Manager is performed at a time, possibly using a semaphore in PSA API.
So, when using Secure Manager, you don't have to deal with secure stack, secure context.
I hope this answers your question
Best regards
Jocelyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-24 9:10 AM
Hello @QuentinWit ,
One example you can use is the X-CUBE-AZURE-H5 here
It is using ThreadX with SecureManager.
Best regards
Jocelyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-25 3:44 AM
Hi,
Here's a wiki that describe what needs to be done to use an RTOS in the Secure Manager context :
https://wiki.st.com/stm32mcu/wiki/Security:How_to_use_an_RTOS_with_Secure_Manager_on_STM32H5
Regards,
Tony
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-03-31 8:55 AM - edited ‎2025-03-31 8:58 AM
Hi
To complement what Jocelyn wrote, in X-CUBE-AZURE-H5 package, see application in Projects\STM32H573I-DK\Applications\ROT\Nx_Azure_IoT. It is a project where ThreadX and the application run in non-secure side.
In this project, see Core\Src\ns_ipc_tx_lock.c for locking the calls to secure manager. It is an example of secure manager access locking with threadx.
Note in the IDE project files that TX_SINGLE_MODE_NON_SECURE is set 1 for both the C compiler and the assembler.
Note that Core\Src\system_stm32h5xx_ns.c is used (not system_stm32h5xx.c). The difference is that SystemInit() does nothing. The clocks are initialised in the secure boot.
There is no need to use tx_thread_secure_stack.c.
Note that an additional timer is started to increment the STM32 HAL tick count. ThreadX reserves the Systick for its own use. See main.c and stm32h5xx_hal_timebase_tim.c.
Also if you plan to use the STM32 RNG IP, the secure manager reserves its use .