Skip to main content
Associate
July 16, 2024
Question

STM32U585xx SBSFU source code examples do not build properly.

  • July 16, 2024
  • 1 reply
  • 799 views

STM32U585xx SBSFU source code examples do not build properly.

Nice to meet you.
If you download and check the en.stm32cubeu5-v1-6-0.zip file (including patch), it contains an example for STM32U585 SBSFU.
If you try to build the 'SBSFU' example for 'B-U585I-IOT02A' board according to the instructions in readme.html, it does not build properly and 'Build failed' occurs, and even if it is built properly, 'SBSFU_Appli\Binary\sbsfu_app.bin' ', etc. are not created.
I would like to solve the problem for some reason, so please give me some advice.
*****
Example source: Refer to STM32Cube_FW_U5_V1.6.0/Projects/B-U585I-IOT02A/Applications/SBSFU/readme.html.
Tools: IAR EWARM 9.50.1
situation :
'SBSFU_Appli\Binary\sbsfu_app.bin' not created.
'SBSFU_Appli\Binary\sbsfu_app_init.bin' not created.
'SBSFU_Appli\Binary\sbsfu_app_enc_sign.bin' not created.
'SBSFU_Appli\Binary\sbsfu_app_sign.bin' not created.

'SBSFU_Loader Non Secure Project' Build failed.
We are unable to proceed because this issue has not been resolved.
Please help.
thank you

This topic has been closed for replies.

1 reply

ST Technical Moderator
August 19, 2024

Hi @Debugger 

There is a known limitation when your path contains spaces:

Known limitations

  • IAR build not working if cube package is installed on a path with a space, or a long path.
  • STM32CubeIDE: Only Release configuration is supported due to flash mapping constraint. To allow debugging in Release configuration, the debug level is -g3.

CMYL_0-1724075178608.png

Can you please double check if your path doesn't contain spaces ?

On my side, I built the projects as described in the Readme w/o any issues. 

best regards