STM32H523 debug authentication, read protection, and product state
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-23 11:42 AM
Hi,
In the past we've always produced 'release' firmware for STM32F4 which checks the RDP level (memory read / debug protection) at boot up, and ensures it's automatically set to RDP1 (read protection enabled). This ensures that our code can't be easily read out of the device by 3rd parties, but if necessary I can connect a debugger, reset the option bytes (which performs a full erase), and reprogram the chip. This works well. We also have our own secure bootloader which deals with encrypted firmware updates and which is well supported by our production equipment and staff.
I'm now working on porting a design to STM32H523, which has an enormously more complicated security system.
What I've figured out so far is that:
- I think the closest behaviour it's capable of would be to have TrustZone disabled, to set a password for Debug Authentication, and to have the product in the "CLOSED" state when shipped.
- This would ensure the product is read protected, but it can be fully erased and set back to the "OPEN" state provided the password is known.
- To make this happen, I need to start with it in the "OPEN" state, somehow transition to "PROVISIONING" because the OBKeys can't be written when it's "OPEN", then write the OBKeys to set the password hash, then transition to "CLOSED".
I've worked through these steps using the STM32CubeProgrammer, and only managed to completely brick one device. I'm honestly pretty happy with that. However, it's an involved, fiddly process that won't work in production.
(Also, if anyone can suggest a way to recover my Nucleo board then I'd appreciate it - it's stuck in the PROVISIONING state, it won't authenticate because the OBKeys aren't programmed, and I can't connect in order to to program them).
Instead, I'd like to have the application itself make the necessary changes as part of its first time boot sequence, ie. on boot-up:
- if the state is "OPEN", change to "PROVISIONING"
- if it's "PROVISIONING", write the OBKeys and change to "CLOSED"
- if it's "CLOSED", run the application as normal.
I've already written code to calculate the OBKeys from the password, and it works (ie. its output matches the OBKeys that are generated by TrustedPackageCreator. However, since I don't want to make a habit of bricking CPUs, there's some things I'd like to check before continuing...
- when I write FLASH_OPTSR_PRG to change PRODUCT_STATE, does this cause a reboot?
- Table 23 in RM0481v3 says that in the PROVISIONING state, it will always boot to RSS instead of my code. Does this mean I need to write something to SBS_RSSCMDR to make it jump back to my code to continue the sequence? I can't find anything that documents what the RSS commands actually are - and, of course, if I issue a reboot and never get back to my application code, the chip is bricked.
- is there a way to test writing the OBKeys area that doesn't involve putting the chip into a state where debugger access is restricted? I'd really like to know this is working before changing PRODUCT_STATE to something from which I can't recover.
- this does all feel convoluted and difficult, compared to just setting RDP = 1. Have I missed something?
Thanks!
Andy.
Solved! Go to Solution.
- Labels:
-
STM32 Security
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-23 1:28 PM
Hello @andy ,
the STM32H523 is a non crypto version. This means OBK are not encrypted. So, it is possible to write the DA OBK in open state.
This can be done by your firmware.
Regarding transition to CLOSED state, this can also be done by firmware itself. Just need to switch to PROVISIONING or IROT PROVISION in a first step, without resetting and then switch to CLOSED.
You can find code example in the github hotspot here
The example provided is for STM32H573 with TZ enabled device, so only part is applicable to your device. You can reuse the code example for transition to CLOSED state. For OBK writing your need to remove the encryption.
I plan to update this github for other H5 devices but too busy right now.
Best regards
Jocelyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-23 1:28 PM
Hello @andy ,
the STM32H523 is a non crypto version. This means OBK are not encrypted. So, it is possible to write the DA OBK in open state.
This can be done by your firmware.
Regarding transition to CLOSED state, this can also be done by firmware itself. Just need to switch to PROVISIONING or IROT PROVISION in a first step, without resetting and then switch to CLOSED.
You can find code example in the github hotspot here
The example provided is for STM32H573 with TZ enabled device, so only part is applicable to your device. You can reuse the code example for transition to CLOSED state. For OBK writing your need to remove the encryption.
I plan to update this github for other H5 devices but too busy right now.
Best regards
Jocelyn
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-25 9:54 AM
Thank you. I have managed to get this working now, though there are a couple of issues with the information in RM0481 (version 3)...
Page 2989 clearly states that:
The debug authentication configuration must be done only when the PRODUCT_STATE is
“Provisioning”, cannot be performed when PRODUCT_STATE is “Open”.
This isn't the case. Computing and programming the OBKeys for debug authentication in the OPEN state works just fine, as you said.
Also, the definition of the data to provision (table 715) isn't quite right. The "SHA256 of the overall blob" actually needs to be computed over the next 64 bytes, not 48, ie. there must be 256 bits reserved and set to 0, in order to match the .obk file produced by TrustedPackageCreator.
On the plus side, I've managed to successfully (recoverably!) lock a production device without bricking any more parts, which is a great way to end on a Friday afternoon. Have a great weekend!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-28 11:59 AM
Hello @andy
This sentence is a bit too generic. It is actually true (or at least partially) when you use a STM32H573, because of the crypto operations used.
In fact this sentence is true in the context of using a tool like STM32CubeProgrammer to provision the obk.
If provisioning is done by firmware, it does not apply.
Thank you for raising RM issue. I will raise a ticket for that.
Good to see you got it working fine :)
Best regards
Jocelyn