cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G0 Readout Protection questions

BrianB
Associate II

1.  If in RDP Level 1, can the SRAM be read?

2.  If starting in RDP Level 1 and transitioning to RDP Level 0, is the SRAM erased?

3.  Can the contents of SRAM be readout after the transition from RDP Level 1 to RDP Level 0?

 

Thanks.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

1) No, RDP level 1 prevents SRAM from being read. From the reference manual:

TDK_1-1703194324512.png

2) Yes.

3) Yes, but they've been erased.

(Assuming you mean "read" as "read by the debugger" as the program itself can use SRAM just fine regardless of RDP level.)

 

Relevant reading material:

https://www.st.com/resource/en/application_note/an5156-introduction-to-stm32-microcontrollers-security-stmicroelectronics.pdfhttps://kolegite.com/EE_library/application_notes/STM32/STM32_Security.pdf

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

1) No, RDP level 1 prevents SRAM from being read. From the reference manual:

TDK_1-1703194324512.png

2) Yes.

3) Yes, but they've been erased.

(Assuming you mean "read" as "read by the debugger" as the program itself can use SRAM just fine regardless of RDP level.)

 

Relevant reading material:

https://www.st.com/resource/en/application_note/an5156-introduction-to-stm32-microcontrollers-security-stmicroelectronics.pdfhttps://kolegite.com/EE_library/application_notes/STM32/STM32_Security.pdf

 

If you feel a post has answered your question, please click "Accept as Solution".
BrianB
Associate II

Thanks for the quick reply