2013-11-11 11:26 AM
Hello
Maybe I'm wrong, but thehttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/PF259409
only provides binaries compatible with compilers from Keil or IAR but none for GCC. Since the sources aren't openly available, for reasons I can understand, is it possible that somebody from ST provides us an GCC compatible version? Thank you. #stm32-cryptograhic-library-gcc #understand-your-tools #understand-your-tools #know-your-tools2016-11-18 9:59 PM
Hi
Thanks for your response and sorry for the late reply.First of all I used 3.1.0 version.SHA256 cryptography HASH algorithm works fine i already tested.Regarding RSA 2048 bits key I didn't found any example key so I can test RSA library.Do you have any RSA2048 bits Private and public key then please share me else share me link so i can generate key from some tools.Thanks & RegardsParesh Parekh2016-11-19 6:12 AM
Could you use OpenPGP or GnuPG to generate some keys?
2016-11-19 6:20 AM
hi,
I have a few basic questions regarding the x-cube-cryptolib + STM32F415RG: 1. Since the cryptlib is declared as a STM32Cube extension, I tried to install the zip over the Library Manager, which results in an invalid version error message (Cube version 4.17.0, Library version: 3.1.0). Is this extension even installable directly in STM Cube? 2. The AccHW HAL driver seems to identical with the files in the firmware directory of my MPU. Is the HW cryptlib extension even necessary for HAL? 3. In the includefiles ''STM32CubeExpansion_Crypto_V3.1.0\AccHw_Crypto\STM32F4\Middlewares\ST\STM32_Crypto_AccHw\Inc'' there are only algorithms that are not supported by the hardware acceleration of my MPU, for example RSA. So at this point the complete cryptlib stopped making sense to me...2016-11-20 11:49 PM
Hi Clive1
Thanks for the quick response, I got the key from www.pgpkeygem.com In ST library if we want to pass private or public keys then key must be have two components Exponential and Modules. How i can identify Exponential and Modules from the current keys. Also here I attached both key generate from the above website. Regards from Paresh Parekh ________________ Attachments : 0xEE98F688-pub.asc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0AQ&d=%2Fa%2F0X0000000bg1%2FqU05PDia7IRZOMVTRGAuINSDJWy8gVNPNnxo42jktbU&asPdf=false0xEE98F688-sec.asc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0wg&d=%2Fa%2F0X0000000bfx%2Fxoy6jQfWiFqYeiFV0G.nkxnbhtQuu4qRkKtAvu20Gcs&asPdf=false