2025-11-05 5:53 AM
Hi,
I am working with the SBSFU_Boot on the STM32U5A9 chip. After the SBSFU_Loader has written the update image into internal memory, a reset happens in order for the SBSFU_Boot to write the image to be booted. When performing the update, it ends up in a process where it has to do some encryption. The SAES engine is initialized successfully, and then AES_Encrypt is called. This keeps on failing because a read error is reported in the SAES->SR reports a read error upon enabling the SAES peripheral.
It should be noted that the initialization and encryption sequence is strictly followed per instructions in RM0456 Rev 6 sections 50.4.4 (Initialization of SAES) and 50.4.8 (ECB/CBC encryption sequence) respectively.
What am I missing?
Solved! Go to Solution.
2026-04-22 11:23 PM
Hi Jocelyn,
It turns out that the SAES wasn't configured correctly. After this was sorted out, it worked.
Best regards,
Mourice.
2025-11-11 6:51 AM
Hello @Mourice ,
From your description it is not clear if you have made adaptations or not.
Could you please provide more details?
Best regards
Jocelyn
2025-11-12 1:16 AM
Hi Jocelyn,
I have not made any adaptations.
Best regards,
Mourice.
2025-11-13 11:28 AM
2025-11-17 4:59 AM
2025-11-28 8:16 AM
Hello @Mourice,
I couldn't reproduce your issue.
I used latest STM32Cube_FW_U5_V1.8.0 as base and followed readme to adapt B-U585I-IOT02A to STM32U5A9J-DK.
It is booting properly and update is working as expected.
I join the adaptation I made so that you can check on your side.
Best regards
Jocelyn
2025-12-04 4:43 AM
Hi Jocelyn,
I will try out your adaptation and give you feedback.
Best regards,
Mourice.
2026-04-22 11:23 PM
Hi Jocelyn,
It turns out that the SAES wasn't configured correctly. After this was sorted out, it worked.
Best regards,
Mourice.