cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5 Traceclock

Sebastian33
Associate II

Hello


I trying to figure out what the maximum frequency is for the TRACECLK  stm32u5A9.
I found this post for the stm32h5

https://community.st.com/t5/stm32-mcus-products/traceclk-freq-in-stm32h5/td-p/604127

does the same apply for stm32u5 were can i in that case find this information for stm32u5?

Are there any pcb layout guidlines for 
TRACECK
TRACED[3:0]

Sebastian33_0-1768552686257.png

 

5 REPLIES 5
KDJEM.1
ST Employee

Hello @Sebastian33 ;

 

I reported this issue internally. I will get back to you with more details as soon as possible.

Internal ticket number: 225506 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Viktor POHORELY
ST Employee

TRACECLK is connected to SYSCLK/2.

Please note that GPIO AC characteristics must be respected - high capacitive load or low voltage may not allow maximum speed of the TRACECLK signal.

FNiel.1
Associate III

I'm the hardware architect on this design. We are matching the impedance of the lines to the tracer connector to be 80Ohm. I assume that that fits the STM32 U5 drive impedance fairly well as this is the impedance of the Segger IDC cable?

We are also matching length as much as possible as per the Segger layout recomendations. 

And length from STM32U5 to Tracer will be aproximately 25 cm including the Segger cable.

Please advise if any line buffers are needed.

TRACECLK is connected to SYSCLK/2.
Can i find this information somewhere in the stm32u5 documentation. Can i find similar information for other stm32 processors?