cancel
Showing results for 
Search instead for 
Did you mean: 

PKA driver: Problems with modular multiplication and exponentiation

elopezpe
Associate II

Hello all,

I have been working on a bare metal Rust implementation of the PKA engine in the STM32WBA55CG microcontroller. So far, I managed to properly initialize the PKA engine, and run both modular addition and subtraction by writing and reading the PKA RAM memory. However, when trying to run modular multiplication and exponentiation, the operation simply never ends (PROCENDF never clears).  I am not sure why could this be, since I am just modifying the mode and the in/out memory offsets to which I write in the RAM. Below I show the corresponding code.

The PKA RAM memory can be found in page 82 of rm0493 (https://www.st.com/resource/en/reference_manual/rm0493-multiprotocol-wireless-bluetooth-le-and-ieee802154-stm32wba5xxx-armbased-32bit-mcus-stmicroelectronics.pdf)

 

 

#![no_std] #![no_main] use stm32wba::stm32wba55::{self}; use {defmt_rtt as _, panic_probe as _}; use cortex_m_rt::entry; use cortex_m::asm; use defmt::info; use core::{ mem::size_of, ptr::{read_volatile, write_volatile}, }; const BASE: usize = 0x520C_2000; const PKA_RAM_OFFSET: usize = 0x400; const RAM_BASE: usize = BASE + PKA_RAM_OFFSET; // PKA RAM locations for exponentiation const EXPONENT_LENGTH_OFFSET: u32 = 0x400; const OPERAND_LENGTH_OFFSET: u32 = 0x408; const OPERAND_A_OFFSET: u32 = 0xC68; const MODULUS_OFFSET: u32 = 0x1088; const EXPONENT_E_OFFSET: u32 = 0xE78; const RESULT_OFFSET: u32 = 0x838; const OPERAND_LENGTH: u32 = 64; const EXPONENT_LENGTH: u32 = 64; const A: u32 = 2; // Base const E: u32 = 3; // Exponent const N: u32 = 13; // Modulus for exponentiation unsafe fn write_ram(offset: usize, buf: &[u32]) { debug_assert_eq!(offset % 4, 0); debug_assert!(offset + buf.len() * size_of::<u32>() < 0x520C_33FF); buf.iter().rev().enumerate().for_each(|(idx, &dw)| { write_volatile((offset + idx * size_of::<u32>()) as *mut u32, dw) }); } unsafe fn read_ram(offset: usize, buf: &mut [u32]) { debug_assert_eq!(offset % 4, 0); debug_assert!(offset + buf.len() * size_of::<u32>() < 0x520C_33FF); buf.iter_mut().rev().enumerate().for_each(|(idx, dw)| { *dw = read_volatile((offset + idx * size_of::<u32>()) as *const u32); }); } #[entry] unsafe fn main() -> ! { let p = stm32wba55::Peripherals::take().unwrap(); let pka = &p.PKA; let clock = &p.RCC; let rng = &p.RNG; // Enable HSI as a stable clock source clock.rcc_cr().modify(|_, w| w .hseon().set_bit() ); while clock.rcc_cr().read().hserdy().bit_is_clear() { asm::nop(); } // Enable RNG clock. Select the source clock clock.rcc_ccipr2().write(|w| w.rngsel().b_0x2()); // Enable RNG clock. Select the AHB clock clock.rcc_ahb2enr().modify(|_, w| w.rngen().set_bit()); while clock.rcc_ahb2enr().read().rngen().bit_is_clear() { asm::nop(); } // Configure RNG rng.rng_cr().write(|w| w .rngen().clear_bit() .condrst().set_bit() .configlock().clear_bit() // .clkdiv().b_0x0() .nistc().clear_bit() // Hardware default values for NIST compliant RNG .ced().clear_bit() // Clock error detection enabled ); // First clear CONDRST while keeping RNGEN disabled rng.rng_cr().modify(|_, w| w .condrst().clear_bit() ); // Then enable RNG in a separate step rng.rng_cr().modify(|_, w| w .rngen().set_bit() .ie().set_bit() ); while rng.rng_sr().read().drdy().bit_is_clear() { asm::nop(); } info!("RNG enabled successfully"); // Enable PKA peripheral clock via RCC_AHB2ENR register // PKA peripheral is located on AHB2 clock.rcc_ahb2enr().modify(|_, w| w.pkaen().set_bit()); // Reset PKA before enabling (sometimes helps with initialization) pka.pka_cr().modify(|_, w| w.en().clear_bit()); for _ in 0..10 { asm::nop(); } // Enable PKA peripheral pka.pka_cr().write(|w| w .en().set_bit() .mode().bits(0x00) ); // Wait for PKA to initialize while pka.pka_sr().read().initok().bit_is_clear() { asm::nop(); } info!("PKA initialized successfully!"); let length_addr = BASE + OPERAND_LENGTH_OFFSET as usize; let exponent_length_addr = BASE + EXPONENT_LENGTH_OFFSET as usize; let operand_a_addr = BASE + OPERAND_A_OFFSET as usize; let exponent_addr = BASE + EXPONENT_E_OFFSET as usize; let modulus_addr = BASE + MODULUS_OFFSET as usize; let result_addr = BASE + RESULT_OFFSET as usize; // Clear any previous error flags pka.pka_clrfr().write(|w| w .addrerrfc().set_bit() .ramerrfc().set_bit() .procendfc().set_bit() ); // Write the values - using 32-bit words write_ram(length_addr, &[OPERAND_LENGTH]); write_ram(exponent_length_addr, &[EXPONENT_LENGTH]); write_ram(operand_a_addr, &[A]); write_ram(operand_a_addr + 4, &[0]); // Additional zero word 4 bytes = 32 bits = 1 word write_ram(exponent_addr, &[E]); write_ram(exponent_addr + 4, &[0]); // Additional zero word write_ram(modulus_addr, &[N]); write_ram(modulus_addr + 4, &[0]); // Configure PKA operation mode and start info!("Starting PKA operation..."); pka.pka_cr().modify(|_, w| w .mode().bits(0x00) .start().set_bit() // Start the operation ); // Wait for processing to complete - PROCENDF is 1 when done info!("Waiting for operation to complete..."); while pka.pka_sr().read().procendf().bit_is_clear() { asm::nop(); } info!("Operation complete!"); // Read the result let mut result = [0u32; 1]; read_ram(result_addr, &mut result); info!("Operation: {} ^ {} (mod {}) = {}", A, E, N, result[0]); // Clear the completion flag pka.pka_clrfr().write(|w| w.procendfc().set_bit()); loop {} }
View more

 

 

 

2 REPLIES 2
Bubbles
ST Employee

Hi @elopezpe,

I'll notify colleagues who work in Rust about your question. Last time I checked they also didn't have PKA support ready, but at least they can notify you about their plans.

BR,

Jarda

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

toromanoSTM
ST Employee

Hello,

I see your new question https://community.st.com/t5/stm32-mcus-wireless/stm32wba55cg-modular-multiplication-not-working/td-p/787945 , so it seems this specific issue (block at waiting PROCENDF)  is now fixed. Can you confirm ?

 

The main difference, I see, is the fn zero_ram() so I suspect a bad ROS/EOS write. (it was the main issue i had when writing some PKA C driver)

https://github.com/STMicroelectronics/optee_os/blob/4.0.0-stm32mp/core/drivers/crypto/stm32/stm32_pka.c
https://github.com/STMicroelectronics/arm-trusted-firmware/blob/v2.10-stm32mp/drivers/st/crypto/stm32_pka.c

Note it was not on the same SOC.

I'll have a look at your new post.

BR,

Nicolas.