2017-10-19 2:21 AM
Hello,
I am using the STM crypto library X-CUBE-CRYPTOLIB (there are several libraries and I could not find out which one was recommended so I picked the most recent one) with an STM32F417.
I can't find any information about the internal implementation. More specifically, I need to know if the AccHw_ AES routines use DMA. The CRYP_IN DMA stream is (2, 6), but my application requires SDIO on the same stream (I can't use stream (2,3) because it is needed by SPI1_TX).
My initial testing shows that the encryption seems to work despite the fact that the SDIO is on and active, but I need to understand *why* does it work and if I can rely on this behaviour.
Therefore, I have the following questions:
- Does X-CUBE-CRYPTOLIB uses DMA for the AES encryption? - If it does, how can it work in parallel with the SDIO? - If it does not, why? Does it uses interrupts? Polling? How can this be optimal?- Can it be configured and how?Thanks for any information that could help me sort this through.
Charles#crypto #dma #aes #x-cube-cryptolib2017-10-23 4:03 AM
Hi
charles.sdn
,X-CUBE-CRYPTOLIB doesn't use DMA for the AES encryption but developed based on polling mode. This is done to keep DMA streams available for other peripherals in the end user's application.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.