Skip to main content
Associate III
October 29, 2024
Question

Hard Fault Issues While Switching to Non-Secure Zone

  • October 29, 2024
  • 3 replies
  • 1219 views

Hello,

I am using the STM32U575ZIT6 microcontroller and have created a simple TrustZone project where all applications run in the non-secure zone. However, when the program attempts to switch to the non-secure zone, it triggers a hard fault handler error, showing the message "no signal source available for 0xfffffff9." I have configured the secure zone as follows:

 

 

#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* Non-secure Vector table to jump to (internal Flash Bank2 here) */
/* Caution: address must correspond to non-secure internal Flash where is */
/* mapped in the non-secure vector table */
#define VTOR_TABLE_NS_START_ADDR 0x08100000UL

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
static void NonSecure_Init(void);
static void MX_GTZC_S_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* SAU/IDAU, FPU and interrupts secure/non-secure allocation setup done */
/* in SystemInit() based on partition_stm32u575xx.h file's definitions. */

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/
 SCB->SHCSR |= SCB_SHCSR_SECUREFAULTENA_Msk;
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();



 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* GTZC initialisation */
 MX_GTZC_S_Init();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOE_CLK_ENABLE();

 __HAL_RCC_GPIOF_CLK_ENABLE();

 __HAL_RCC_GPIOG_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 HAL_GPIO_ConfigPinAttributes(GPIOA, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOB, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOC, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOD, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOE, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOF, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOG, GPIO_PIN_ALL, GPIO_PIN_NSEC);
 HAL_GPIO_ConfigPinAttributes(GPIOH, GPIO_PIN_ALL, GPIO_PIN_NSEC);

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /*************** Setup and jump to non-secure *******************************/

 NonSecure_Init();

 /* Non-secure software does not return, this code is not executed */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief Non-secure call function
 * This function is responsible for Non-secure initialization and switch
 * to non-secure state
 * @retval None
 */
static void NonSecure_Init(void)
{
 funcptr_NS NonSecure_ResetHandler;

 SCB_NS->VTOR = VTOR_TABLE_NS_START_ADDR;

 /* Set non-secure main stack (MSP_NS) */
 __TZ_set_MSP_NS((*(uint32_t *)VTOR_TABLE_NS_START_ADDR));

 /* Get non-secure reset handler */
 NonSecure_ResetHandler = (funcptr_NS)(*((uint32_t *)((VTOR_TABLE_NS_START_ADDR) + 4U)));

 /* Start non-secure state software application */
 NonSecure_ResetHandler();
}

/**
 * @brief GTZC_S Initialization Function
 * None
 * @retval None
 */
static void MX_GTZC_S_Init(void)
{

 /* USER CODE BEGIN GTZC_S_Init 0 */

 /* USER CODE END GTZC_S_Init 0 */

 MPCBB_ConfigTypeDef MPCBB_Area_Desc = {0};

 /* USER CODE BEGIN GTZC_S_Init 1 */

 /* USER CODE END GTZC_S_Init 1 */
 MPCBB_Area_Desc.SecureRWIllegalMode = GTZC_MPCBB_SRWILADIS_ENABLE;
 MPCBB_Area_Desc.InvertSecureState = GTZC_MPCBB_INVSECSTATE_NOT_INVERTED;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[0] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[1] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[2] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[3] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[4] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[5] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[6] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[7] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[8] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[9] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[10] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[11] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[12] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[13] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[14] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[15] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[16] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[17] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[18] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[19] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[20] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[21] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[22] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[23] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[24] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[25] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[26] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[27] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[28] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[29] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[30] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[31] = 0x00000000;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[0] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[1] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[2] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[3] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[4] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[5] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[6] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[7] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[8] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[9] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[10] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[11] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[12] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[13] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[14] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[15] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[16] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[17] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[18] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[19] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[20] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[21] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[22] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[23] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[24] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[25] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[26] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[27] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[28] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[29] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[30] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[31] = 0xFFFFFFFF;
 MPCBB_Area_Desc.AttributeConfig.MPCBB_LockConfig_array[0] = 0x00000000;
 if (HAL_GTZC_MPCBB_ConfigMem(SRAM3_BASE, &MPCBB_Area_Desc) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN GTZC_S_Init 2 */

 /* USER CODE END GTZC_S_Init 2 */

}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

 

 

 

 

 

 

 

 

 

 

 

This topic has been closed for replies.

3 replies

Frantz LEFRERE
ST Technical Moderator
November 4, 2024

Hello @Istillaga ,
have you set the flash watermark option byte  ? 

- SECWM1_PSTRT=0x0 SECWM1_PEND=0x7F meaning all 128 pages of Bank1 set as secure
- SECWM2_PSTRT=0x7F SECWM2_PEND=0x0 meaning all 128 pages of Bank2 set as non_secure

 

IstillagaAuthor
Associate III
November 4, 2024

Yes, I have configured the flash byte watermark option but instead of 0x7f in SECWM2_PSTR I have set the value to 0x1

Frantz LEFRERE
ST Technical Moderator
November 4, 2024

I would suggest to check code example provided in the CubeFW:
STM32Cube_FW_U5_V1.6.0\Projects\NUCLEO-U575ZI-Q\Examples\GPIO\GPIO_IOToggle_TrustZone

If you still faced an issue please share your complete project.