2025-01-06 05:02 PM
Hi,
I have enabled the HASH, RNG, and PKA. I also enabled the Global Trust Zone Controller and configured the PKA as privilege access. However, the generated code from STM32CubeMX does produce an error due to undefined
GTZC_CFGR3_PKA_Pos which is missing from stm32h523xx.h
Is that an error?
I have to mention that when I first created the project, I haven't check Trust Zone option under the project. But I later enabled the GTZC.
Kind Regards,
Hani
Solved! Go to Solution.
2025-01-22 10:59 AM
Hello @hakeila ,
According to the internal ticket feedback :
will be published in 25W08 on ST.COM H5 CubeFW v1.5.0
Best regards
Jocelyn
2025-01-22 12:28 PM
Hi @Jocelyn RICARD,
Thank you for the quick reply.
Is there an ETA for releasing the CubeFw 1.5.0?
Regards,
Hani