cancel
Showing results for 
Search instead for 
Did you mean: 

GTZC and PKA privileged config

hakeila
Associate III

Hi,

 

I have enabled the HASH, RNG, and PKA. I also enabled the Global Trust Zone Controller and configured the PKA as privilege access. However, the generated code from STM32CubeMX does produce an error due to undefined 

GTZC_CFGR3_PKA_Pos which is missing from stm32h523xx.h

 

Is that an error? 

 

I have to mention that when I first created the project, I haven't check Trust Zone option under the project. But I later enabled the GTZC.


Kind Regards,

Hani

12 REPLIES 12
Jocelyn RICARD
ST Employee

Hello @hakeila ,

According to the internal ticket feedback :

will be published in 25W08 on ST.COM H5 CubeFW v1.5.0

Best regards

Jocelyn

Hi @Jocelyn RICARD,

 

Thank you for the quick reply.

Is there an ETA for releasing the CubeFw 1.5.0?

 

Regards,

Hani

Jocelyn RICARD
ST Employee

Yes week 8 as stated above

Best regards

Jocelyn