cancel
Showing results for 
Search instead for 
Did you mean: 

Executing an application directly from RAM rather than the flash memory - SBSFU.

Hotaru
Associate

We currently utilize the STM32H7B0xB microcontroller, which offers 1.4 MBytes of RAM and 128KBytes of flash memory. While exploring the SBSFU examples found examples for running from external flash directly, I could not locate one that specifically demonstrates running the application from the RAM region for SBSFU. Is it supported?

2 REPLIES 2
MM..1
Chief II

Thanks @MM..1  for running the code from RAM. However, I was looking at secure boot and if SBSFU supports apps running app after doing a signature verification and decryption.