cancel
Showing results for 
Search instead for 
Did you mean: 

Error when installing secure firmware image to STM32U585

abhkr241
Associate

Hello,

I generated an SFI image for STM32U585 based on my application.  here is the details:

Firmware information:

abhkr241_1-1736985173277.png

SFI image details:

abhkr241_0-1736985052857.png

However, when I try to install this image, it fails with the error:
15:12:04:987 : PROGRAMMING OPTION BYTES AREA ...
  15:12:05:267 : Database: Config 11 is active.
  15:12:05:267 : Warning: Option Byte: TZEN, value: 0x1, was not modified.
  15:12:05:267 : Warning: Option Byte: nBoot0, value: 0x0, was not modified.
  15:12:05:267 : Warning: Option Byte: nSWBoot0, value: 0x0, was not modified.
  15:12:05:267 : Warning: Option Bytes are unchanged, Data won't be downloaded
  15:12:05:267 : Time elapsed during option Bytes configuration: 00:00:00.280
  15:12:05:275 : Programming via Debugger!
  15:12:05:331 : Programming via Debugger!
  15:12:05:399 : Programming via Debugger!
  15:12:05:467 : Programming via Debugger!
  15:12:05:536 : Execute RSS get version Payload...
  15:12:05:545 : Programming via Debugger!
  15:12:05:609 : halt ap 0
  15:12:05:616 : run ap 0
  15:12:05:616 : halt ap 0
  15:12:05:616 : RSS version = 1.4.0
  15:12:05:617 : Reading STM32 descriptor ...
  15:12:05:621 : STM32 Descriptor successfully read
  15:12:05:621 : Get RSSe version...
  15:12:05:625 : Programming via Debugger!
  15:12:05:682 : Programming via Debugger!
  15:12:05:742 : Programming via Debugger!
  15:12:05:800 : Programming via Debugger!
  15:12:05:864 : Execute RSS get version Payload...
  15:12:05:868 : Programming via Debugger!
  15:12:05:933 : halt ap 0
  15:12:05:942 : run ap 0
  15:12:05:943 : halt ap 0
  15:12:05:943 : RSSe version = 4.0.0
  15:12:05:943 : Starting SFI
  15:12:05:943 : Processing license...
  15:12:06:051 : Programming via Debugger!
  15:12:06:128 : Programming via Debugger!
  15:12:06:205 : Programming via Debugger!
  15:12:06:273 : Programming via Debugger!
  15:12:06:337 : Execute Process License payload...
  15:12:06:340 : Programming via Debugger!
  15:12:06:407 : halt ap 0
  15:12:06:418 : run ap 0
  15:12:07:113 : halt ap 0
  15:12:07:114 : Succeed to execute Process License payload...
  15:12:07:114 : Get RSSe status...
  15:12:07:125 : Programming via Debugger!
  15:12:07:198 : Programming via Debugger!
  15:12:07:274 : Programming via Debugger!
  15:12:07:350 : Programming via Debugger!
  15:12:07:426 : Execute RSSe Get Status Payload...
  15:12:07:504 : Programming via Debugger!
  15:12:07:580 : halt ap 0
  15:12:07:589 : run ap 0
  15:12:07:589 : halt ap 0
  15:12:07:589 : Succeed to execute RSSe Get Status ...
  15:12:07:589 : Processing Image Header
  15:12:07:590 : Writing Img header to address 0x20040300
  15:12:07:596 : Programming via Debugger!
  15:12:07:668 : Programming via Debugger!
  15:12:07:738 : Programming via Debugger!
  15:12:07:813 : Programming via Debugger!
  15:12:07:892 : Execute Process Image Header payload...
  15:12:07:896 : Programming via Debugger!
  15:12:07:976 : halt ap 0
  15:12:07:981 : run ap 0
  15:12:07:983 : halt ap 0
  15:12:07:984 : Succeed to execute RSSe Process Image Header payload...
  15:12:07:984 : Get RSSe status...
  15:12:07:994 : Programming via Debugger!
  15:12:08:066 : Programming via Debugger!
  15:12:08:127 : Programming via Debugger!
  15:12:08:198 : Programming via Debugger!
  15:12:08:274 : Execute RSSe Get Status Payload...
  15:12:08:353 : Programming via Debugger!
  15:12:08:438 : halt ap 0
  15:12:08:446 : run ap 0
  15:12:08:446 : halt ap 0
  15:12:08:447 : Succeed to execute RSSe Get Status ...
  15:12:08:447 : Processing Area 1...
  15:12:08:452 : Programming via Debugger!
  15:12:08:588 : Programming via Debugger!
  15:12:08:656 : Programming via Debugger!
  15:12:08:722 : Programming via Debugger!
  15:12:08:795 : Execute Process Area payload for Area 1...
  15:12:08:799 : Programming via Debugger!
  15:12:08:874 : halt ap 0
  15:12:08:883 : run ap 0
  15:12:09:521 : halt ap 0
  15:12:09:524 : Succeed to execute Process Area payload for Area 1...
  15:12:09:525 : Get RSSe status...
  15:12:09:525 : Programming via Debugger!
  15:12:09:608 : Programming via Debugger!
  15:12:09:687 : Programming via Debugger!
  15:12:09:768 : Programming via Debugger!
  15:12:09:841 : Execute RSSe Get Status Payload...
  15:12:09:923 : Programming via Debugger!
  15:12:09:991 : halt ap 0
  15:12:09:999 : run ap 0
  15:12:09:999 : halt ap 0
  15:12:09:999 : Succeed to execute RSSe Get Status ...
  15:12:09:999 : Area Address = 0x8000000
  15:12:09:999 : Area Type    = F
  15:12:09:999 : Processing Area 2...
  15:12:10:000 : Programming via Debugger!
  15:12:10:058 : Programming via Debugger!
  15:12:10:120 : Programming via Debugger!
  15:12:10:184 : Programming via Debugger!
  15:12:10:248 : Execute Process Area payload for Area 2...
  15:12:10:248 : ---- Is Last SFI Area !! ----
  15:12:10:254 : Programming via Debugger!
  15:12:10:313 : halt ap 0
  15:12:10:319 : run ap 0
  15:12:10:335 : halt ap 0
  15:12:10:335 : Error: Execution of RSS CMD failed, returned value = 0x1

 

- The license part looks ok to me.

I am not able to determine if there is an issue with my firmware image or the way I am generating my image. 
Any help would be appreciated. Thanks!

0 REPLIES 0