cancel
Showing results for 
Search instead for 
Did you mean: 

CRC Calculation for 8-bit values

BILLyTheLiTTle
Associate II

I am experimenting with CRC Calculation on a STM32F4-Discovery.

As I have seen in the reference manual this MCU is using CRC-32 used in Ethernet. I am also using https://crccalc.com/ (CRC-32/MPEG-2) to validate the results.

I just activate the CRC in CubeMX and this is my source code for 32-bit values:

uint32_t raw_data_32_bit[BUFFER_SIZE] = { 0x00, 0x01, 0x10, 0x1A, 0xAC, 0xC0 };
uint32_t crc_value_32_bit = 0;
uint8_t is_error_32_bit = 1;
 
crc_value_32_bit = HAL_CRC_Calculate(&hcrc, raw_data_32_bit, BUFFER_SIZE);
  if (crc_value_32_bit == expected_crc_value_32_bit) {
	  is_error_32_bit = 0;
  }

which is working like a charm.

Then I would like to do the same for 8-bit values with this code:

uint32_t expected_crc_value_8_bit = 0xA4541FC6;
uint8_t raw_data_8_bit[BUFFER_SIZE] = { 0x00, 0x01, 0x10, 0x1A, 0xAC, 0xC0 };
uint32_t crc_value_8_bit = 0;
uint8_t is_error_8_bit = 1;
 
crc_value_8_bit = HAL_CRC_Calculate(&hcrc, (uint32_t *) raw_data_8_bit, BUFFER_SIZE); // returns 0xe7206456
  if (crc_value_8_bit == expected_crc_value_8_bit) {
	  is_error_8_bit = 0;
  }

but it returns a different result from the result returns from https://crccalc.com/. The only way to make it work is to create a new 32-bit array using this code:

uint32_t data [BUFFER_SIZE];
for (uint8_t i = 0; i < BUFFER_SIZE; i++)
   data[i] = raw_data_8_bit[i];
 
 
crc_value_8_bit = HAL_CRC_Calculate(&hcrc, data, BUFFER_SIZE); 
if (crc_value_8_bit == expected_crc_value_8_bit) {
   is_error_8_bit = 0;
}

Could someone explain why the 8-bit returns something different from the expected? What am I doing wrong?

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
waclawek.jan
Super User

In the first case, you calculate CRC from an array of {0x1A100100, 0xqqqqC0AC, 0xqqqqqqqq, 0xqqqqqqqq, 0xqqqqqqqq, 0xqqqqqqqq}, where qq are whatever bytes happen to be in the memory just after raw_data_8_bit[].

In the second case, you calculate CRC from {0x00000000, 0x000000001, 0x00000010, 0x0000001A, 0x000000AC, 0x000000C0}

+1

sizeof() the arrays is different, the function is taking a word count, not a byte count.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@Community member​ 

I thought that the conversion

(uint32_t *) raw_data_8_bit

converts the pointer of an 8-bit value into a 32-bit value pointer.

Maybe I have not understand something in pointer functionality. If you could, I would like a more detailed explanation or even some keywords for a google search in order to read an article.

@Community member​ 

Wow! So, is there any way (apart from the third code snippet) to calculate CRC on an 8-bit array?

In this video here, it seems it is working as expected!

@everyone

Thank you for your time.

Yes that casts the pointer but 8 words is still 32 bytes​, not 8

Check the units used by HAL_CRC_Calculate() and use the right ones..​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User

In C, information on variable's *type* is *not* passed to the called function. Rather, the value passed is used according to whatever type is declared for that parameter in the function's declaration.

JW

Gumer RoMa
Associate III

I think you should initialize the CRC using the right parameters for a 8 bit CRC.

Here is an example:

HAL_StatusTypeDef CRC_configure_CDMA2000(){

hcrc.Instance = CRC;

hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_DISABLE;

hcrc.Init.DefaultInitValueUse = DEFAULT_INIT_VALUE_DISABLE;

hcrc.Init.GeneratingPolynomial = 0x9b;

hcrc.Init.CRCLength = CRC_POLYLENGTH_8B;

hcrc.Init.InitValue = 0xff;

hcrc.Init.InputDataInversionMode = CRC_INPUTDATA_INVERSION_NONE;

hcrc.Init.OutputDataInversionMode = CRC_OUTPUTDATA_INVERSION_DISABLE;

hcrc.InputDataFormat = CRC_INPUTDATA_FORMAT_BYTES;

return HAL_CRC_Init(&hcrc);

}

And then use the CRC as follows:

uint8_t crc_data[4] = {0x1A, 0x2B, 0x3C,0x4D};

uint32_t crc_result;

crc_result = HAL_CRC_Calculate(&hcrc, (uint32_t*)crc_data, 4);

Hope this helps,

Gumer

The thread is over a year old, and discusses a STM32F4 part that doesn't support a programmable CRC peripheral, so only ST's 32-bit one.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..