2022-04-22 12:07 AM
@Jocelyn RICARD We need secure storage to keep Private Keys and certificates for TLS communication on STM32H753.
To achieve this we found STSAFE-A110, but interfacing and to bring in this peripheral, it is time taking in terms of re-spin PCB design etc.
Instead of this, can we choose PCROP protection mechanism, like converting Data to Instructions with help of scripts and then store them under PCROP protections ??
is this solution looks feasible ??
Solved! Go to Solution.
2022-04-25 1:46 AM
In fact, there are different needs.
Secure User memory is here to prevent the user application from accessing the SBSFU code and assets. It can be seen as a "temporal isolation" : when the bootloader has finished its job then its area "disappears".
Now, when SBSFU runs, we also have a "regional isolation" between the secure part of the SBSFU (Secure Engine: dealing with the assets) and the non-secure part (for instance the loader using the UART must not access the assets as the UART might be used as an attack point).
Now, why PCROP ?
In fact the idea is to have some "mutual distrust", even in the secure enclave.
We trust the code in Secure Engine but, if unfortunately there is a flaw in this code allowing to dump the FLASH then the PCROP protects us.
It is really the idea of building a fortified solution with layered security.
SBSFU:
User Application:
But, PCROP must be used with code only (no D fetch allowed).
So, the PCROP-ed code loads the key in RAM.
Hence, there is a window of time where the key is in RAM.
But, only Secure Engine can use it.
As always, there might always be vulnerabilities but the intention is to make it very complex to exploit it.
2022-04-25 4:42 AM
@Jocelyn RICARD Your perspective on this Please ??
2022-04-25 4:48 AM
Looks like my reply has not been posted...sorry for this...
Basically STSAFE-A110 will bring you:
It has the constraint of having the I2C secure channel so a pair of MAC/Cipher keys.
You will need to diversify it per device.
Now, I need to check with an STSAFE-A110 expert but I think you can configure STSAFE-A110 so that your private key never goes out of the secure element, even if somebody steals the MAC/Cipher keys.
This is what you would gain.
But, if you do not protect the MAC/Cipher keys then somebody might spoof the STM32 and ask the STSAFE-A110 to do some operations.
Probably here you may put under PCROP the code dealing with STSAFE-A110 and storing the MAC/Cipher keys.
This way the keys would not be dumped from FLASH.
I will ask an STSAFE-A110 expert his view.
Let's say that we still have assets to protect on STM32 side: the MAC and Cipher keys.
But, your most important asset, the private key, would not be exposed to leakage.
2022-04-25 4:52 AM
It is really a matter of security level you want to achieve.
MPU-based isolation has some limits (applies only to the Cortex-M master + requires to deprivilege your application).
PCROP and WRP protect FLASH only.
So, STSAFE-A110 can bring many benefits:
Now, if the level of protection provided by MPU and PCROP/WRP is sufficient for you, for sure it can work. You just need to assess the limits of these mechanisms versus your security requirements.
2022-04-25 4:55 AM
Looks like I am facing issues to post...testing...
2022-04-25 4:58 AM
@Fred I am getting your posts, as you asked Jocelyn for confirmation, i have just added him to the discussion.
Thanks for your valuable replies.
2022-04-26 2:10 AM
Hello,
I discussed with the STSAFE-A110 experts.
So, this is what the STSFE-A110 can bring as additional benefits compared to an STM32H7-only solution:
So, this means that we could protect the pairing key on the STM32H7 side to avoid STM32 spoofing that would allow an attacker to send commands to the STSAFE-A110.
But, if our security mechanisms are circumvented by the attacker, still he cannot extract your private key from the STSAFE-A110.
More information about STSAFE-A110 personalization can be found here:
STSAFE-A110 generic sample profile description - Application note
Again, I do not mean that STSAFE-A110 is mandatory, STM32H7 already brings a level of security, but with STSAFE-A110 you can go one step further if it is critical for you to protect the private key.
2022-04-26 2:53 AM
Another option could also be to:
As you can see, many options are possible.
It also depends heavily on the attacks you want to thwart.
2022-04-26 11:44 PM
@Fred To provision STSAFE-A110, We won't share our private keys with ST. We want to provision STSAFE in our secure environment, is this allowed ??
STSAFE-A110, is the device used to store certificates, which is used to establish TLS communication, which means for example, wolfSSL will read these key details to initiate TLS handshake. Without keys, it is difficult.
Then what is the real use case of STSAFE ??
@Jocelyn RICARD can you help with the storage of Pairing Keys mechanism ??
2022-04-27 12:06 AM
I will forward your questions to our STSAFE-A110 experts but here are my 2 cents:
If you want an example of STSAFE-A110 usage in an IoT use-case, you can have a look at this presentation:
https://www.youtube.com/watch?v=uMheyCl3vas&list=PLnMKNibPkDnF0oofZPLdyEnUg2BpfBS8p&index=1
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.