2026-01-17 6:23 AM - last edited on 2026-01-19 1:16 AM by Saket_Om
Hi team,
I am working with the STM32H7S78-DK board and implementing TLS 1.3 using WolfSSL on the client side.
Project setup:
Board: STM32H7S78-DK
TLS library: WolfSSL (TLS 1.3 enabled)
Network: TCP client socket
Server: OpenSSL TLS 1.3 server
Certificates: Public and private keys generated and configured
issue:
I am able to create the TCP client socket successfully, but when I attempt to establish a secure TLS connection with the OpenSSL server, the handshake fails.
Handshake error: -308
1)What does the WolfSSL handshake error -308 indicate during a TLS 1.3 connection?
2)What are the possible causes of this error when communicating with an OpenSSL TLS 1.3 server?
Any suggestions, references, or troubleshooting steps to resolve this issue would be very helpful.
Thank you for your support.
thanks & regards,
Karthik.