cancel
Showing results for 
Search instead for 
Did you mean: 

Zero crossing detection

Krishna36
Associate

HELLO, 

Can you please suggest us any mcu having internal block for zero crossing detection in stm32 for 50 - 60hz frequency signals or any slave chips that are dedicated for zero crossing detection.

 

Thank you, 

Krishna. 

 

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @Krishna36, to the community!

This is a recurring question for which you will find several entries here in the community, e.g. this one.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Uwe Bonnes
Chief

How large is your 50 Hz? What is your timing requirement?

Probably you can use a STM32 with comparator and use the 50 Hz offset to about half the supply voltage compared to half the supply voltage. I would use an external comparator with common mode input to some - 100 mV put a fitting resistor in the 50 Hz line, clip the voltage with two antiparallel schottky diode and compare against ground.