cancel
Showing results for 
Search instead for 
Did you mean: 

X value of BOOT1 pin

dps
Associate II
Posted on February 12, 2009 at 04:50

X value of BOOT1 pin

2 REPLIES 2
jilisegiar
Associate II
Posted on May 17, 2011 at 13:02

it means don't care

dps
Associate II
Posted on May 17, 2011 at 13:02

Hello.

I want to start application from User Flash memory.

I must connect BOOT_0 pin to log. 0............. OK

But, is it possible to connect BOOT1 pin to log. 0, too ?

In datasheet's table it is state ''X'' for BOOT_1 pin and log.0 for BOOT0_0 pin.

What ''X'' mean ?

1. Unconnected float pin (Hi-Z)

or

2. don´t care (log.1 or log.0)

Is it possible to run application from User Flash memory with this configuration: BOOT_0 = log. 0, BOOT_1 = log.0 ?

Thanks