2018-10-15 11:46 PM
Hi guys,
I’m new with x-cube sbsfu package and I have some troubles with running the example on stm32l476. I saw the stm manual for getting started etc but it didn’t work for me. Can anyone explain how to import properly project into workspace in Atollic and what should I do next in steps? I know that example is for sw4stm32 but it should also work in atollic, so please give me some tips how to properly run this on stm32l476. I didn’t have any problems with other stm32 packages but this one is hard one for me to run.
Best regards
2019-04-11 7:58 PM
(I use the SW4STM32 converted by TrueSTUDIO)
10:20:34 **** Incremental Build of configuration Debug for project STM32L476RG_NUCLEO_2_Images_SECoreBin ****
Info: Internal Builder is used for build
arm-atollic-eabi-gcc -c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -g -Wa,--warn -x assembler-with-cpp -specs=nano.specs -o Application\User\se_key.o ..\..\se_key.s
arm-atollic-eabi-gcc -c ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_Secure_Engine\Core\se_crypto_common.c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -std=gnu11 -DSTM32L476xx -DUSE_HAL_DRIVER -DUSE_STM32L4XX_NUCLEO
....(I remove the long log here)
Generate build reports...
Print size information
text data bss dec hex filename
18386 80 2616 21082 525a SECoreBin.elf
Print size information done
Generate listing file
Output sent to: SECoreBin.list
Generate listing file done
Generate build reports done
arm-atollic-eabi-objcopy -O binary SECoreBin.elf SECoreBin.bin
10:20:40 Build Finished (took 5s.867ms)note: I copy the prebuild.bat and SECBOOT_AES128_GCM_AES128_GCM_AES128_GCM.bat from \2_Images_SECoreBin\MDK-ARM to \2_Images_SECoreBin\SW4STM32
=======================================================================
10:56:34 **** Rebuild of configuration Debug for project STM32L476RG_NUCLEO_2_Images_SECoreBin ****
Info: Internal Builder is used for build
prebuild.bat C:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\2_Images_SECoreBin\SW4STM32\
Prebuild with windows executable
複製了 1 個檔案。
arm-atollic-eabi-gcc -c ..\..\data_init.c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -std=gnu11 -DSTM32L476xx -DUSE_HAL_DRIVER -DUSE_STM32L4XX_NUCLEO -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\Linker_Common\SW4STM32 -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../../../../../../../../Drivers/STM32L4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32L4xx_Nucleo -I../../../../../../../../Drivers/BSP/Components/Common -I../../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32L4/Inc -I../../../../../../../../Middlewares/ST/STM32_Secure_Engine/Core -I../../../../../../../../Middlewares/ST/STM32_Secure_Engine/Key -I../../../../../../../../Drivers/CMSIS/Include -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\2_Images_SECoreBin\Inc -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\2_Images_SBSFU\SBSFU\App -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -Wno-strict-aliasing -specs=nano.specs -o Application\SW4STM32\data_init.o
arm-atollic-eabi-gcc -c ..\..\..\Src\se_crypto_bootloader.c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -std=gnu11 -DSTM32L476xx -DUSE_HAL_DRIVER -DUSE_STM32L4XX_NUCLEO -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\Linker_Common\SW4STM32 -I../../../Inc -I../../../../../../../../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../../../../../../../../Drivers/STM32L4xx_HAL_Driver/Inc -I../../../../../../../../Drivers/BSP/STM32L4xx_Nucleo -I../../../../../../../../Drivers/BSP/Components/Common -I../../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32L4/Inc -I../../../../../../../../Middlewares/ST/STM32_Secure_Engine/Core -I../../../../../../../../Middlewares/ST/STM32_Secure_Engine/Key -I../../../../../../../../Drivers/CMSIS/Include -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\2_Images_SECoreBin\Inc -IC:\X-CUBE-SBSFU_V2.1.0\Projects\NUCLEO-L476RG\Applications\2_Images\2_Images_SBSFU\SBSFU\App -Os -ffunction-sections -g3 -fstack-usage -Wall -fmessage-length=0 -Wno-strict-aliasing -specs=nano.specs -o Application\User\se_crypto_bootloader.o
arm-atollic-eabi-gcc -c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -g -Wa,--warn -x assembler-with-cpp -specs=nano.specs -o Middlewares\STM32_Secure_Engine\se_stack_smuggler_GNU.o ..\..\..\..\..\..\..\..\Middlewares\ST\STM32_Secure_Engine\Core\se_stack_smuggler_GNU.s
arm-atollic-eabi-gcc -c -mthumb -mcpu=cortex-m4 -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -g -Wa,--warn -x assembler-with-cpp -specs=nano.specs -o Application\User\se_key.o ..\..\se_key.s
..\..\se_key.s: Assembler messages:
..\..\se_key.s:1: Error: bad instruction `area |.SE_Key_Data|,CODE'
..\..\se_key.s:2: Error: bad instruction `export SE_ReadKey'
..\..\se_key.s:3: Error: bad instruction `se_readkey'
..\..\se_key.s:13: Warning: this instruction will write back the base register
..\..\se_key.s:17: Error: bad instruction `export SE_ReadKey_Pub'
..\..\se_key.s:18: Error: bad instruction `se_readkey_pub'
..\..\se_key.s:28: Warning: this instruction will write back the base register
..\..\se_key.s:38: Warning: this instruction will write back the base register
..\..\se_key.s:48: Warning: this instruction will write back the base register
..\..\se_key.s:58: Warning: this instruction will write back the base register
..\..\se_key.s:61: Error: bad instruction `end'
10:56:37 Build Finished (took 2s.976ms)What 's going on ???
compiler settings issue from TrueSTUDIO or ... anything missed to configure ?