2008-02-14 07:02 AM
working I2C code for IAR KickStartâ„¢ kit for STM32
2011-05-17 03:23 AM
Hello!
Im looking for working sample code for the IAR KickStartâ„¢ kit for STM32. There is example 1-5 in one of the folders that is followed with the IAR software but none of them works for me. I need something easy to send data on the I2C1 bus, interrupt would also be nice so it will get information when some pin on the stm32 get low it download data from a temperature sensor or something like that. Its kinda strange that its isnt any good demo code on this for study purpose.