WKUP2 Operation on STM32L152-EVAL
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2012-08-02 8:12 AM
Posted on August 02, 2012 at 17:12
Hello, I'm hoping someone can either confirm or deny what I as seeing.
I've modified the PWR STANDBY example to check the working of all three WKUP pins.I seem to have a problem when I enable WKUP2.If I only enable WKUP1 & WKUP3 then both work as expected, but when I enable all three then none them work. All I have done is to add in the additional calls to PWR_WakeupPinCmd as below: PWR_WakeUpPinCmd(PWR_WakeUpPin_1, ENABLE); PWR_WakeUpPinCmd(PWR_WakeUpPin_3, ENABLE); PWR_WakeUpPinCmd(PWR_WakeUpPin_2, ENABLE); If I comment out the third call that enabled WKUP2 then WKUP1 & 3 work again.Even if the PC13 line was being pulled high or low by the eval board I would not expect it to prevent the other two from working.Can anyone shed any light on this.Thanks. #wkup2-stm32l152-eval-pc13
Labels:
- Labels:
-
Power
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0