2012-05-31 11:16 AM
I successfully compiled the stm3240g Sample Project using Code Sourcery.
But, it does nothing on the Discovery Board.But, this code is directly converted from as WORKING Code on the Discovery Board
- when compiled with Atollic Compiler.-> Why should the Code not run successfully if it compiles by the Code Sourcery too ??
What could cause this problem - difference ? Would WinArm work any better ?2012-06-14 2:48 PM
With -Os optimization enabled, and removing extraneous source files I've gotten it down to about a 15KB binary. It's hard faulting on my F2, so will try the F4-Discovery next.
The GNU linker is not good at ejecting useless code, the trick I think is to put all the ST fw library objects (.o) into an library file (.a) and then the linker will cherry pick the things it actually needs. Edit: Ok I have the 6MB ELF downloaded (15KB active), connecting via CN5 I have ''STM microSD Flash USB Device'' showing up in Device Manager on Win7 Pro 64-bit. I can download/debug via Keil by replacing a donor .AXF file in an existing project.2012-06-15 12:20 PM
I did a quick port of the STM322XG_EVAL to my board this morning. Had to mod the LEDs and Card Detect pin assignments, and stripped out the LCD stuff. It is successfully accessing a 2GB SD card.
Tools : Yagarto MAKE 3.81 Yagarto GNU/GCC 4.6.2 STM32 USB Library, which actually contains a newer version of the FW library. As for general development, commercially we have ARM Realview for the older ARM9 SoC designs, Keil for some STR7, STR9, and STM32 work. I also have an older Rowley seat (1.6 or 1.7) for a design that used STR7 and the vendor wanted that. For MIPS and SPARC SoC I've used GNU/GCC, being cheap and vendor supported. I've got some ATMEL ARM9 stuff that builds with older WinARM (GNU 4.0 or 4.3), and some STM32F1 and F2 (M3) that will work with that too. Yagarto 4.6.2 seems to be the way to go for Cortex-M4, I could probably fight that back to some other versions. I don't have a problem using any particular tool chain and OS, the trick is often to use one that is contemporaneous to the source code being compiled, and not to mix-and-match different versions, or ABI models. I have to build kernels in Linux, but most everything I'd prefer to use Windows, if for no other reason that I have a large arsenal of tools I can bring to bear. I haven't looked at the SD speed, the things aren't terrible rapid.2012-06-25 11:27 AM
The speed is mostly limited by the 12 Mbps USB Full Speed rate. It will also be impacted by the Class of SDHC card. There can be some significant performance difference between cards claiming to be 4, 6, and 10, and sequential and random access.
Project source has been posted here [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Where is the UsbMassStorage Examples Supt for stm32f4xx&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=249]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fWhere%20is%20the%20UsbMassStorage%20Examples%20%20Supt%20for%20stm32f4xx&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy.st.com%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FAllItems.aspx¤tviews=249