2021-02-24 9:51 PM
Hello i am using Nucleo F746ZG board. When i run simple LED blink code with below code its not showing LD5 (Over current) on.
#include "mbed.h"
// Blinking rate in milliseconds
#define BLINKING_RATE 500ms
int main() {
// Initialise the digital pin LED1 as an output
DigitalOut led(LED1); // Green Color
while (true) {
led = !led;
ThisThread::sleep_for(BLINKING_RATE);
}
}But when i changed code given below LD5(Over Current) blinking. and also controller heating is too much.
#include "mbed.h"
// Blinking rate in milliseconds
#define BLINKING_RATE 500ms
int main() {
// Initialise the digital pin LED1 as an output
DigitalOut led(LED1); // Green Color
while (true) {
led = !led;
}
}Reason behind checking this code is my main code was showing Over current LED ON, so i changed code to LED Blink, and found this issue. Looks like Nucleo board having issue for continuous operation. I have Connected SD card Module with SDMMC CN8 , when i remove SD card module from SDMMC its not showing over current.Can someone please help?
2021-03-17 2:04 AM
There are several values listed in the Datasheet.
2021-03-17 2:34 AM
I am talking about Table 15. Current characteristics ΣIIO value in datasheet because nucleo board showing overcurrent. 120 mA is sum of all GPIO current, Right?