2018-01-25 1:19 AM
hi guys.
i wrote a code with IAR , and when is run the code in stm32f103ret , cpu go to the interrupt s routin.
i dont know why??!!i want to have 1msecond delay for each timer priode , but i cant do that. when the code runs , cpu go to interrupt routine fanction. i do some thing that i know. but i cant do this activity. this is my code:who know why I cant??
so thanks.#include 'stm32f10x.h'
#include 'stm32f10x_gpio.h' // for Enable LCD#include 'stm32f10x_rcc.h' //for Enable LCD#include 'stm32f10x_tim.h'#include 'LCDLib.h'#include 'delay.h'void tim_init(void);void GPIO_init(void);void TIM1_UP_TIM16_IRQHandler (void){ int i; i = TIM_GetPrescaler(TIM1); lcdGoxy(1 , 2); lcdPutInt(i); lcdGoxy(1 , 3); lcdPutString ('tim activated'); TIM_ClearITPendingBit(TIM1,TIM_IT_Update);}int main(){ lcd_init(); tim_init(); GPIO_init(); while(1){ } }void tim_init(){ RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 55000; TIM_TimeBaseStructure.TIM_Prescaler = 55999; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure); TIM_ITConfig(TIM1, TIM_IT_Update, ENABLE); NVIC_InitTypeDef NVIC_InitStructure; /* Enable the TIM2 global Interrupt */ NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);}void GPIO_init(void){ RCC_APB2PeriphClockCmd ( RCC_APB2Periph_GPIOA, ENABLE ); GPIO_InitTypeDef gpioA; gpioA.GPIO_Mode = GPIO_Mode_Out_PP ; gpioA.GPIO_Pin = GPIO_Pin_0; gpioA.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init ( GPIOA, &gpioA ); }Solved! Go to Solution.
2018-01-27 2:05 PM
&sharpinclude 'stm32f10x.h'
&sharpinclude 'stm32f10x_gpio.h' // for Enable LCD&sharpinclude 'stm32f10x_rcc.h' //for Enable LCD&sharpinclude 'stm32f10x_tim.h'&sharpinclude 'LCDLib.h'&sharpinclude 'delay.h'void tim_init(void);void GPIO_init(void);void TIM1_UP_IRQHandler(void) // assuming startup_stm32f103xe.s pulled
{ static int i = 0;if (TIM_GetITStatus(TIM1, TIM_IT_Update) == SET)
{ TIM_ClearITPendingBit(TIM1,TIM_IT_Update);GPIOA->ODR ^= GPIO_Pin_0; // Toggle PA0
lcdGoxy(1 , 2);
lcdPutInt(i++); // Incrementing countlcdGoxy(1 , 3);
lcdPutString ('tim activated'); }}void TIM1_UP_TIM16_IRQHandler(void) // if startup_stm32f10x_hd_vl.s being pulled
{ TIM1_UP_IRQHandler();}int main(){ RCC_ClocksTypeDef RCC_Clocks; uint32_t j;lcd_init();
lcdPutString ('Believe Your Dreams.');tim_init();
GPIO_init();RCC_GetClocksFreq(&RCC_Clocks);
j = (RCC_Clocks.PCLK2_Frequency/1000);
lcdGoxy(1 , 4);
lcdPutInt(j);GPIO_WriteBit(GPIOA, GPIO_Pin_0, Bit_SET);
while(1){
}
}void tim_init()
{ NVIC_InitTypeDef NVIC_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
/* Enable the TIM1 global Interrupt, before we enable it on TIM */
NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = 36000 - 1; // KHz, take 36 MHz clock to 1 KHz TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // Hz (1) 1000 ticks of 1 KHz clock TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);/* TIM1 enable counter */
TIM_Cmd(TIM1, ENABLE);/* Enable the update interrupt */
TIM_ITConfig(TIM1, TIM_IT_Update, ENABLE);}void GPIO_init(void)
{ GPIO_InitTypeDef gpioA;RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
gpioA.GPIO_Mode = GPIO_Mode_Out_PP;
gpioA.GPIO_Pin = GPIO_Pin_0; gpioA.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init (GPIOA, &gpioA);}2018-01-25 7:33 AM
TIM1_UP_IRQn not equivalent to TIM1_UP_TIM16_IRQHandler, needs some coherency.
Check the name in the vector table in startup_stm32f1xxx.s if there is no linkage, the function isn't going to get called.
If using .CPP files, makes sure to use extern 'C' so the names aren't mangled.
2018-01-27 7:11 AM
thanks.
i change to tim2 . and i change startup file (got it from cube).but cant slove my problem.i test many ways,i dont know what do i do !!!!
do you have any seggestions for me??thanks you.
2018-01-27 7:30 AM
You test many ways but show next to no detail. What file? What are the vectors in it? Consider ZIPing up a project and attaching so the context can be understood.
The sample shown looks to come from SPL rather than Cube/HAL
The TIM divides down 36 MHz, it will interrupt every 85 seconds, not 1 ms
TIM1_UP_IRQHandler would be expected with
TIM1_UP_IRQn
2018-01-27 1:09 PM
thanks.
i just want to have delay from timer counter of stm32. i mean when the counter overflows , then i have an interrupt and in function of interrupt i do somethings.
i wrote code but i dont know when i init the timer/counter , interrupt happened and cpu do the interrupt routin code with no delay.
i havent any delay with timer/counter.
i saw a lot of example and the code was same but the code of mine dosent work.
i use stm32f103ret and IAR.
this is my project file :
so thanks.
2018-01-27 2:05 PM
&sharpinclude 'stm32f10x.h'
&sharpinclude 'stm32f10x_gpio.h' // for Enable LCD&sharpinclude 'stm32f10x_rcc.h' //for Enable LCD&sharpinclude 'stm32f10x_tim.h'&sharpinclude 'LCDLib.h'&sharpinclude 'delay.h'void tim_init(void);void GPIO_init(void);void TIM1_UP_IRQHandler(void) // assuming startup_stm32f103xe.s pulled
{ static int i = 0;if (TIM_GetITStatus(TIM1, TIM_IT_Update) == SET)
{ TIM_ClearITPendingBit(TIM1,TIM_IT_Update);GPIOA->ODR ^= GPIO_Pin_0; // Toggle PA0
lcdGoxy(1 , 2);
lcdPutInt(i++); // Incrementing countlcdGoxy(1 , 3);
lcdPutString ('tim activated'); }}void TIM1_UP_TIM16_IRQHandler(void) // if startup_stm32f10x_hd_vl.s being pulled
{ TIM1_UP_IRQHandler();}int main(){ RCC_ClocksTypeDef RCC_Clocks; uint32_t j;lcd_init();
lcdPutString ('Believe Your Dreams.');tim_init();
GPIO_init();RCC_GetClocksFreq(&RCC_Clocks);
j = (RCC_Clocks.PCLK2_Frequency/1000);
lcdGoxy(1 , 4);
lcdPutInt(j);GPIO_WriteBit(GPIOA, GPIO_Pin_0, Bit_SET);
while(1){
}
}void tim_init()
{ NVIC_InitTypeDef NVIC_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM1, ENABLE);
/* Enable the TIM1 global Interrupt, before we enable it on TIM */
NVIC_InitStructure.NVIC_IRQChannel = TIM1_UP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;NVIC_Init(&NVIC_InitStructure);
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Prescaler = 36000 - 1; // KHz, take 36 MHz clock to 1 KHz TIM_TimeBaseStructure.TIM_Period = 1000 - 1; // Hz (1) 1000 ticks of 1 KHz clock TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseStructure.TIM_RepetitionCounter = 0; TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);/* TIM1 enable counter */
TIM_Cmd(TIM1, ENABLE);/* Enable the update interrupt */
TIM_ITConfig(TIM1, TIM_IT_Update, ENABLE);}void GPIO_init(void)
{ GPIO_InitTypeDef gpioA;RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
gpioA.GPIO_Mode = GPIO_Mode_Out_PP;
gpioA.GPIO_Pin = GPIO_Pin_0; gpioA.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init (GPIOA, &gpioA);}2018-01-28 3:33 AM
i am realy thank you.
you help me a lot.thanks.