cancel
Showing results for 
Search instead for 
Did you mean: 

how can i get value from IN1 and IN2 from ADC in CMSIS

hossein hosseini
Associate II
Posted on December 18, 2017 at 21:20

hi.

i wrote a code for ADC1 , and i could get value from ADC1_channel_1 (IN1)  but i cant get value of Channel_2 and show both of two value  on LCD in same time.

I dont know which function can I use to get both value . in this code i have just Channel_1 value .

i use IAR and stm32f103RE.

(i know the code is long , but i sholud put it for you , so thanks)

&sharpinclude 'stm32f10x.h'

&sharpinclude 'stm32f10x_gpio.h'  // for Enable LCD

&sharpinclude 'stm32f10x_rcc.h'   //for Enable LCD

&sharpinclude 'stm32f10x_adc.h'

&sharpinclude 'LCDLib.h'

&sharpinclude 'delay.h'

void init_adc(void);

int adcValue = 5000 ;

int main()

{

  init_adc();

  lcd_init();

  lcdPutString ('Believe Your Dreams.');

   

  while(1){

    

   ADC_SoftwareStartConvCmd(ADC1, ENABLE);

   adcValue = ADC_GetConversionValue(ADC1);

   

   lcdGoxy( 1 ,  3);

   lcdPutString ('           ');

   lcdGoxy( 1 ,  3);

   lcdPutInt(adcValue);

  

   delay_ms(200);  

   ADC_SoftwareStartConvCmd(ADC1, ENABLE);

   adcValue = ADC_GetConversionValue(ADC1);

   

   lcdGoxy( 1 ,  4);

   lcdPutString ('           ');

   lcdGoxy( 1 ,  4);

   lcdPutInt(adcValue);

   

   delay_ms(200);   

  }

}

void init_adc(void){

 

    GPIO_InitTypeDef GPIO_InitStructure;

    ADC_InitTypeDef ADC_InitStructure;

    RCC_ADCCLKConfig (RCC_PCLK2_Div6);

        

    /* Enable ADC1 and GPIOA clock */

    RCC_APB2PeriphClockCmd ( RCC_APB2Periph_GPIOA | RCC_APB2Periph_ADC1 ,    ENABLE ) ;

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;

    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructure);

    ADC_InitStructure.ADC_ContinuousConvMode = DISABLE;

    ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

    ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;

    ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;

    ADC_InitStructure.ADC_NbrOfChannel = 2;

    ADC_InitStructure.ADC_ScanConvMode = DISABLE;

    ADC_Init(ADC1, &ADC_InitStructure);

    ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_13Cycles5);

    ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 2, ADC_SampleTime_13Cycles5);

        

    ADC_Cmd ( ADC1 , ENABLE ) ;

      

    ADC_ResetCalibration(ADC1);

    while(ADC_GetResetCalibrationStatus(ADC1));

    ADC_StartCalibration(ADC1);

    while(ADC_GetCalibrationStatus(ADC1));

        

        

}

#adc1
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
hossein hosseini
Associate II
Posted on January 28, 2018 at 11:39

we can use DMA to get all of the channels value.