Why does HAL_UART_Receive keep crashing?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-26 4:32 AM
Hi. Can someone please help me see where I am going wrong? The program will transmit the UART message but crashes when it gets to the 'HAL_UART_Receive' function. I am using the STM32F746 Discovery Board.
UART_HandleTypeDef MobileGNSSUartHandle;
uint8_t UART_Rx_Buffer[100];uint8_t UART_Tx_Buffer[] = 'AT\r';GPIO_InitTypeDef GPIO_InitStruct;
HAL_Init(); /* Peripheral clock enable */ __HAL_RCC_USART6_CLK_ENABLE(); /**USART6 GPIO Configuration PC7 ------> USART6_RX PC6 ------> USART6_TX */ GPIO_InitStruct.Pin = GPIO_PIN_6 | GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_USART6; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);// Enable GPIOs clock
__HAL_RCC_GPIOC_CLK_ENABLE();// Initialise UART6
MobileGNSSUartHandle.Instance = USART6; MobileGNSSUartHandle.Init.BaudRate = 115200; MobileGNSSUartHandle.Init.WordLength = UART_WORDLENGTH_8B;; MobileGNSSUartHandle.Init.StopBits = UART_STOPBITS_1; MobileGNSSUartHandle.Init.Parity = UART_PARITY_NONE; MobileGNSSUartHandle.Init.Mode = UART_MODE_TX_RX; MobileGNSSUartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE; MobileGNSSUartHandle.Init.OverSampling = UART_OVERSAMPLING_16; MobileGNSSUartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; MobileGNSSUartHandle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; HAL_UART_Init(&MobileGNSSUartHandle);HAL_UART_Transmit( &MobileGNSSUartHandle, (uint8_t *)UART_Tx_Buffer, 3, 5000 );
HAL_UART_Receive( &MobileGNSSUartHandle, (uint8_t *)UART_Rx_Buffer, 4, 5000 );- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-09-26 6:25 AM
The program will transmit the UART message but crashes when it gets to the 'HAL_UART_Receive' function.
Can you be more specific than that? Does the function return with timeout, or a HardFault is raised, or what? Can you provide the contents of the USART's status register to see if a communication error is present?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-10-07 4:42 PM
Hi.
I ended up figuring out this problem. I needed to do the following:
1. GPIOC needs to be enabled before the pins are configured.
2. To make the timeout of HAL_UART_xxx() work I needed to provide a tick to the HAL.Since the SysTick Handler is also used by embOS, it is defined in RTOSInit_STM32F7x_CMSIS.c, add HAL_IncTick() after OS_TICK_Handle()./* Peripheral clock enable */
__HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_USART6_CLK_ENABLE(); /**USART6 GPIO Configuration PC7 ------> USART6_RX PC6 ------> USART6_TX */ GPIO_InitStruct.Pin = GPIO_PIN_6; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_USART6; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_USART6; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);// Initialise UART6
MobileGNSSUartHandle.Instance = USART6; MobileGNSSUartHandle.Init.BaudRate = 115200; MobileGNSSUartHandle.Init.WordLength = UART_WORDLENGTH_8B; MobileGNSSUartHandle.Init.StopBits = UART_STOPBITS_1; MobileGNSSUartHandle.Init.Parity = UART_PARITY_NONE; MobileGNSSUartHandle.Init.Mode = UART_MODE_TX_RX; MobileGNSSUartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE; MobileGNSSUartHandle.Init.OverSampling = UART_OVERSAMPLING_16; MobileGNSSUartHandle.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; MobileGNSSUartHandle.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if(HAL_UART_DeInit(&MobileGNSSUartHandle) != HAL_OK) { SEGGER_RTT_WriteString(0, 'ERROR: Failed to de-initialize UART!\r\n'); } if(HAL_UART_Init(&MobileGNSSUartHandle) != HAL_OK) { SEGGER_RTT_WriteString(0, 'ERROR: Failed to initialize UART!\r\n'); }