cancel
Showing results for 
Search instead for 
Did you mean: 

Why do some register( USB_OTG_LIB ) not in the (stm32F105/107 ) datasheet?

love21cz
Associate
Posted on May 03, 2010 at 08:16

Why do some register( USB_OTG_LIB ) not in the (stm32F105/107 ) datasheet?

1 REPLY 1
Andrew Neil
Evangelist III
Posted on May 17, 2011 at 13:49

Which particular register(s) are you thinking of?

Note that the actual ''Datasheet'' document is just physical parameters - it's the ''User Manual'' that contains register descriptions, etc...