2015-06-17 8:31 AM
I am working with the
Discovery development board
STM32F407 microcontroller and building using Eclipse/GNU. I have successfully created a small application can communicate with a PC via UART4 and it has free space for a bootloader:MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
STARTUP_VECTOR (rx) : ORIGIN = 0x08000000, LENGTH = 1K
BOOTLOADER (rx) : ORIGIN = 0x08000400, LENGTH = 63K
FLASH (rx) : ORIGIN = 0x08010000, LENGTH = 960K
FLASHB1 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB0 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB1 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB2 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB3 (rx) : ORIGIN = 0x00000000, LENGTH = 0
MEMORY_ARRAY (xrw) : ORIGIN = 0x20002000, LENGTH = 32
}
In the area where the bootloader will reside,
for now, I
simply put a jump-to-the-application:.startUpVector : ALIGN(4)
{
KEEP(*(.startUpVector))
*(.startUpVector .startUpVector.*)
} >STARTUP_VECTOR
.jumpToApplication : ALIGN(4)
{
KEEP(*(.jumpToApplication))
*(.jumpToApplication .jumpToApplication.*)
} >BOOTLOADER
#define JMP(addr) \
__asm__(''mov pc,%0'' \
: /*output*/ \
: /*input*/ \
''r'' (addr) \
);
__attribute__ ((section(''.startUpVector''),used)) pHandler __startUpVector[] =
{
(pHandler) &_estack, // The initial stack pointer
(pHandler) 0x08000401, // The reset handler
};
void __attribute__ ((section(''.jumpToApplication''),used)) __jumpToApplication(void)
{
JMP(0x08010004);
}
In my main.c file I modify theVector Table Offset Register appropriately and everything works like a charm:
SCB->VTOR = 0x08010000;
However, I would like to move my application 4 bytes:
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
CCMRAM (xrw) : ORIGIN = 0x10000000, LENGTH = 64K
STARTUP_VECTOR (rx) : ORIGIN = 0x08000000, LENGTH = 1K
BOOTLOADER (rx) : ORIGIN = 0x08000400, LENGTH = 63K
FLASH (rx) : ORIGIN = 0x08010004, LENGTH = 983036
FLASHB1 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB0 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB1 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB2 (rx) : ORIGIN = 0x00000000, LENGTH = 0
EXTMEMB3 (rx) : ORIGIN = 0x00000000, LENGTH = 0
MEMORY_ARRAY (xrw) : ORIGIN = 0x20002000, LENGTH = 32
}
__attribute__ ((section(''.startUpVector''),used)) pHandler __startUpVector[] =
{
(pHandler) &_estack, // The initial stack pointer
(pHandler) 0x08000401, // The reset handler
};
void __attribute__ ((section(''.jumpToApplication''),used)) __jumpToApplication(void)
{
JMP(0x08010008);
}
SCB->VTOR = 0x08010004;
When I do so, my interrupts stops working. Could someone please give me clue about what's wrong? And another question, what is the correct location to jump to from my bootloader, is it the first address in the interrupt table (''The initial stack pointer'') or the 4th (''The reset handler'')? It seems to work with both, but I suppose that's just luck.
2015-06-17 8:47 AM
Yeah, I really don't think you've grasped the vector table thing at all well. Might I recommend the review of the Cortex-M4 TRM, and one of Joseph Yiu's books?
SCB->VTOR = 0x08010004;
The vector TABLE needs to reside on a 512-byte aligned boundary. Processor isn't using an ADD, but rather using the high-order bits and replacing the low-order bits with the index it wants.The Second Entry, the 32-bit word at +4, is the address of the routine that performs the ResetHandler function, it in turn should initialize the system [SystemInit()], the C memory arena, and transfer control to your main() function.2015-06-17 8:47 AM
SCB->VTOR = 0x08010004;
Read PM0214
, ch.4.4.4 VTOR JW2015-06-18 2:23 AM
Thanks for your post.
2015-06-18 2:25 AM
Thanks. For a while now I've had a feeling I am lacking some documentation and it was exactly the document you referred to.