cancel
Showing results for 
Search instead for 
Did you mean: 

While setting up the clock, if I set PLLM as 8 and PLLN as 360 , it gives same result as when I set PLLM as 4 and PLLN as 180, so what difference does it makes.

SMand.2
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
gbm
Principal

If both sets of values lie within the allowed range (including the VCO max frequency) - there is not a big difference. Higher VCO freq will result in higher power consumption by PLL.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

Depends where the sweet-spot is for the PLL comparison frequency. For the F2/F4 I think it was suggested in the 1-2 MHz region.

Also the VCO likely has a preferred operating range, ie 100 - 432 MHz.

Check the DM and RM

Typically you divide down the VCO frequency to get a square wave into the MCU

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..