cancel
Showing results for 
Search instead for 
Did you mean: 

which stm32 microcontroller has maximum SPI interconnectivity ports

Aanil.1
Associate II

i need to interact with 10sensors which can be connected threw SPI bus alone. so i was looking for a microcontroller where i can hook all 10 SPI sensors

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

When the sensors provide a unique address it is not a matter of the number of SPI ports, but the number of chip selects.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.