cancel
Showing results for 
Search instead for 
Did you mean: 

Which mcu requires the lowest voltage to initialize? Can we do better than an STM32G07KBU6? What is this a function of? Is it: memory size, type of ARM core, number of connected pins ...

ABlak.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The minimum voltage of an STM32 depends on both the technology used and the respective test scope in production. For the latter reason, a minimum voltage of 2.0V is often guaranteed for so-called value line products.

However, you will find many STM32s that can be used from 1.65V: STM32F0, F3, L0, L1, while some members of one family so far is also guaranteed to work from 1.62V: STM32H7. Just open STM32CubeMX, activate the column Voltage Min in the MCU selector and you can choose your favourite.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.