cancel
Showing results for 
Search instead for 
Did you mean: 

Where to report bugs in forum itself?

Osto
Senior
Posted on November 01, 2014 at 13:57

Hi,

This forum (seems to be based on MS-sharepoint) has a lot of bugs.

For example, I can write new discussion only in Chrome and reply only on IE.

When I write a new discussion or reply, I have always to select all and copy to clipboard because 90% of relies/new messages are lost if I dont do that.

Where is to report such bugs?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
frankmeyer9
Associate II
Posted on November 01, 2014 at 19:58

Where is to report such bugs?

 

Seems, it doesn't matter.

People complaining right here about this shaky forum software for years, but nothing has happened yet ...

Perhaps there is some hope.

Early this year, ST released the ''rather immature'' CubeMX software, and since then, forum participation of ST staff has risen manifold. Assuming they experience the same problems firsthand, I hope their complaints are closer to the source ...

Posted on November 02, 2014 at 02:19

It's got a lot of issues, I don't expect it to be fixed. It doesn't work with mobile devices*, and you always have to watch that it doesn't time out your session when you're composing or replying to things. It goes through periods of flakiness, perhaps with phases of the moon, or sunspots.

*Microsoft doesn't appear to understand mobile, or forums.

IoBT - Internet of Broken Things(tm)(sm)
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..