2024-10-29 2:34 PM
I got STM's libraries, grabbed the X-CUBE-DSPDEMO & AN4841 & AN4891 (section 3 on FFT demonstration) but haven't seen any documentation on the DSP library API.
Have all the examples which are great, but still a good documentation for reference would be great.
The AN4891 in section 3 mentions a demo project that runs on MDK-ARM, kind of an FFT performance demonstration. Is that source available somewhere on STM's website or github repo?
Thanks
Solved! Go to Solution.
2024-10-29 3:20 PM
Dear @armDevCP ,
CMSIS-DSP library documentation is made by our Partner ecosystem ARM here : CMSIS-DSP: Overview
Full Github sources are here : CMSIS-DSP/Documentation at main · ARM-software/CMSIS-DSP · GitHub
Source code of the our STM32 X-CUBE-DSPDEMO - Digital Signal Processing with STM32, software expansion for STM32Cube (AN4841) - STMicroelectronics then go to the Software section.
Ciao
STOne-32.
2024-10-29 3:20 PM
Dear @armDevCP ,
CMSIS-DSP library documentation is made by our Partner ecosystem ARM here : CMSIS-DSP: Overview
Full Github sources are here : CMSIS-DSP/Documentation at main · ARM-software/CMSIS-DSP · GitHub
Source code of the our STM32 X-CUBE-DSPDEMO - Digital Signal Processing with STM32, software expansion for STM32Cube (AN4841) - STMicroelectronics then go to the Software section.
Ciao
STOne-32.